点播式网络研讨会

通过集成式端到端结构开发流程加快适航认证

预估观看时长:46 分钟

分享

通过集成式端到端结构开发流程加快适航认证

Aircraft manufacturers can suffer major delays on their programs due to non-recurring costs spent on structural development. Knowing that up to 60% of aircraft non-recurring costs can be spent on the structural development and achieving airworthiness certification, any improvement will have a significant impact.

This webinar discusses how Bye Aerospace (BA) is developing their all-electric eFlyer 2 using an integrated end-to-end structural development process, which helps achieve faster certification. More specifically, BA will show how a model-based primary structure use case is coupled with BA-developed innovative design techniques that enable shorter multidisciplinary design cycles. This speedup is possible through seamless exchange of design and analysis data.

Additionally, we will show how such an integrated end-to-end process can be extended to:

  • Margin of safety calculations with traceable certification reports
  • Flutter simulation tied to the CAD model
  • Material characterization, particularly for composite structures to virtually characterize the material behaviors and significantly reduce composite material development time

主讲嘉宾简介

Bye Aerospace

Daniel Hinson

首席复合材料结构工程师

相关资源

进行生产仿真以改进流程和效率,将人员需求减少 60%
Case Study

进行生产仿真以改进流程和效率,将人员需求减少 60%

瑞健医疗使用 Plant Simulation 通过自动化流程来优化自动注射器的制造物流

将模拟生产流程所需的时间从几天缩短到仅需单击一个按钮
Case Study

将模拟生产流程所需的时间从几天缩短到仅需单击一个按钮

米其林使用 Plant Simulation 和 Mendix 将动态制造仿真用于工业生产