온디맨드 웨비나

Digital image correlation for aircraft materials and structural testing

Gain new insights with digital image correlation (DIC)

예상 소요 시간: 60분

공유

Digital technologies and instruments involved with digital image correlation for aircraft materials and structural testing in aviation

More advanced materials such as composites are used in modern aircraft design for their lightweight properties. Characterizing the mechanical behavior of such complex materials and structures under load is a key enabler in optimizing aircraft designs and reaching the desired strength. One of the challenges of standard measurement techniques, though, is that they only provide limited and local information.

The fast development of digital camera technology in combination with high-performance digital image correlation (DIC) techniques is currently bringing a radical change in this domain and enabling a more efficient and more detailed characterization of materials and structures. DIC enables the identification of mechanical properties of materials by measuring displacement and strain of material samples on dedicated testing machines.

This solution fits into verification processes that need to run when new materials are being considered for aircraft. The Simcenter digital image correlation capabilities support in that context the verification management digital thread within the Siemens Xcelerator portfolio.

In this webinar, we address the following topics for simulation and testing teams:

  • Instrumentation and full-field measurement process
  • Materials testing and identification
  • Structural testing and structural dynamics testing
  • Digital twin validation processes

Benefits of digital image correlation in aviation

Thanks to DIC, it is now possible to extract full-field 3D geometry, displacement, strain and acceleration under any load and for almost any type of aircraft material, with limited instrumentation. These data are crucial in the materials engineering process, as they allow identifying material properties, validating numerical models and assessing the strength of materials and components without the risk of overlooking key local phenomena.

The technology is also applicable to analyze aircraft structural vibrations and dynamic responses. It can be used to characterize rotating and lightweight structures that would otherwise be extremely difficult to test with standard techniques.

Why is digital image correlation important?

Digital image correlation is important to manage increasing complexity in aircraft materials and structures. New issues related to composites, superalloy, lattice structures and more are adding to the complexity. There is a need for faster and more accurate design and verification techniques. DIC provides a new paradigm in materials and structural testing.

How is digital image correlation used in aerospace?

We explain how DIC is used in aerospace, discussing its main applications:

  • Materials testing and identification (coupon test)
  • (Quasi) Static and dynamic testing of structures
  • How to use full-field measurement data to validate a digital twin

Watch the video to learn more.

발표자 소개

Siemens Digital Industries Software

Raphael Hallez

Aerospace Business Development Manager, Simcenter Testing Solutions

Raphael Hallez는 Siemens Digital Industries Software에서 20년 가까이 근무하고 있으며 항공우주 및 방위 기업을 위한 다양한 테스트 및 시뮬레이션 프로젝트에 참여해 왔습니다. 현재는 Simcenter 테스트 솔루션의 비즈니스 개발 활동을 담당하고 있습니다.

MECATEST

Stéphanie Duchesne Sailly, PhD

CEO

After 20 years spent in the world of testing and simulation, Stéphanie created MECATEST to promote the link between physical testing and digital simulation. With her experience acquired at MTS Systems, Hexagon MSC Software, and with numerous automotive stakeholders, she facilitates the use of digital image correlation in various industries.

관련 자료

다차원 시뮬레이션을 활용하여 전기차의 출시 기간과 프로토타입 루프를 단축하는 방법
Case Study

다차원 시뮬레이션을 활용하여 전기차의 출시 기간과 프로토타입 루프를 단축하는 방법

GKN Automotive는 Simcenter Amesim을 사용하여 차세대 eDrive 기술을 최적화합니다

디지털 트윈을 통한  차량 전기화에 대한 엔지니어링 영향
White Paper

디지털 트윈을 통한 차량 전기화에 대한 엔지니어링 영향

다중 영역, 다중 물리 시뮬레이션을 아우르는 포괄적 디지털 트윈으로 비용 및 전기차 R&D 제어