オンデマンド・ウェビナー

Xperi®: A Designer’s Life with HLS

視聴時間の目安: 10 分

共有

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection that they know well with RTL for comparison. The second is to use HLS to develop new Neural Network accelerators and how HLS could help them get from algorithm to critical FPGA demonstrators in a time that would not be possible with traditional RTL flow.

This webinar is part 8 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • Customer's experience using HLS for Image Processing and AI
  • Using HLS for algorithms such as Face Detection with RTL for
    comparison
  • How to use HLS to develop new Neural Network accelerators
  • How HLS can help get from algorithm to critical FPGA demonstrators
    faster than with traditional RTL flow

関連情報

要件と納期を遵守する最適なPLM戦略
E-book

要件と納期を遵守する最適なPLM戦略

この電子ブックでは、エンジニアリング企業にとっての上位の課題 -- 製品要件への適合 (53%) と納期の遵守 (45%) -- に対応する5つの戦略を説明します。

PLMとは何か。なぜクラウド型PLMなのか。
Infographic

PLMとは何か。なぜクラウド型PLMなのか。

PLMとは何かコスト効果が高く高速のクラウド型Teamcenter Xを導入すると、革新的な製品を市場にいち早く投入できます。その詳細をご覧ください。詳細情報

Teamcenter X SaaS PLMの迅速な導入
Video

Teamcenter X SaaS PLMの迅速な導入

使いやすさとアクセス性に優れたTeamcenter X Software-as-a-Service製品ライフサイクル管理 (SaaS PLM) をぜひお試しください。