Webinar on-demand

Complexity in the automotive industry with a systems engineering approach

Tempo di visione stimato: 63 minuti

Condividi

Vehicle engineers using Model-based Systems Engineering (MBSE) approach that helps automotive manufacturers remain competitive, agile, and cost-effective

This webinar discusses how adopting Model-based Systems Engineering (MBSE) helps automotive manufacturers remain competitive, agile, and cost-effective while tackling challenges such as quality, increased regulation, sustainability, and cost. Illustrated with the example of an electric drive, our automotive MBSE experts will explain how to overcome challenges and ensure that the digital thread of requirements remains in the modeling environment from requirements to design, analysis, verification and validation. Register to watch now!

Overcome quality, increased regulation, sustainability, and cost challenges using MBSE

The automotive industry's increased product and process complexity urge many automotive OEMs and suppliers to reevaluate their current product development processes. Deploying a Model-based Systems Engineering (MBSE) approach, connects systems engineering with the rest of the development organization, improving collaboration and decision-making. While the advantages are plentiful, a systems engineering approach encounters challenges: only some requirements can be modeled with the level of accuracy needed, and a heterogeneous mix of modeling and analysis tools from various sources makes it difficult to link all of them synchronously.

Using the example of an electric drive, MBSE experts illustrate how to link all requirements to the corresponding models, ensuring a digital thread of requirements in the modeling environment from requirements to design, analysis, verification and validation.

  • In the early stages: to make an informed decision and arrive at a baseline architecture and refined system requirements that later become a blueprint for detailed design and simulation.
  • In the connected engineering stage: to enable a better product architecture and design options exploration, optimization, and concept selection, including performance evaluation and design trade-offs.
  • In the connected engineering and product validation stage: to ensure that the simulation and testing workflows are well integrated with requirements, system architecture, ECAD/MCAD, and the rest of the process, making it easier to understand and communicate the design and requirements of the electric drive system throughout the development organization.

Key takeaways:

  • Ensure compliance with regulations and standards
  • Reduce risk and increase innovation using a digital thread that remains in the modeling environment
  • Improve collaboration and decision-making based on integrated simulation and testing workflows
  • Obtain a better product architecture, explore design options, and evaluate the performance and trade-offs
  • Improve efficiency and effectiveness by tracking the entire development process, reducing errors, and rework

Register now and learn how to remain competitive, agile, and cost-effective while tackling the challenges of quality, increased regulation, sustainability, and cost.

Relatori

Siemens Digital Industries Software

Vijay Singh

MBSE Solution Consultant

Singh is an MBSE expert consultant in the industry strategy team of the simulation and test solutions segment. In this role, he is responsible for enabling industry-leading customers to successfully integrate their simulation and test workflows as part of their enterprise MBSE solution.

Siemens Digital Industries Software

Steven Dom

Director Automotive Industry Solutions

Steven Dom ha lavorato per Siemens Industry Software (ed ex LMS International) per oltre 20 anni, occupandosi di varie aree ingegneristiche, ingegneria gestionale, gestione dei prodotti e vendite. Attualmente è Director Automotive Industry Solutions, responsabile dello sviluppo delle attività di Siemens Industry Software nell'industria automobilistica, con particolare attenzione a:

Gestione internazionale delle relazioni con i clienti a livello manageriale ed esecutivo

  • Sviluppo di una roadmap strategica tra le divisioni software, hardware e servizi
  • Consulenza in materia di tecnologia e processi aziendali
  • Focus sullo sviluppo di veicoli ibridi ed elettrici
  • Ruolo di consulenza per NVH, acustica ed efficienza energetica

Risorse correlate

Comfort e sicurezza della cabina nelle attrezzature pesanti
White Paper

Comfort e sicurezza della cabina nelle attrezzature pesanti

Le soluzioni intelligenti di Siemens permettono di migliorare la cabina dei macchinari pesanti, con un impatto positivo sul comfort e la sicurezza dell'operatore, riducendo al contempo i tempi di sviluppo.

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico
Case Study

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico

Haulotte usa Simcenter per aumentare l'altezza massima di lavoro dell'unità di sollevamento Pulseo del 25% e la capacità di carico del 50%

Progettazione ad alte prestazioni con il software di modellazione predittiva
Video

Progettazione ad alte prestazioni con il software di modellazione predittiva

Gestire la complessità meccatronica e migliorare il processo progettuale utilizzando software di modellazione predittiva. Maggiori informazioni