Along with the stacks and stacks of data that organizations are generating and must manage, the deep foundation of established systems and solutions is not only highly protected, it adds to the challenge of digital transformation. Often the things that are holding manufacturers back are the things that can’t be compromised. With low-code applications, organizations can finally make use of the data while keeping the core systems clean to produce the analytics that have been missing. Finally, the gaps of the ecosystem can be filled with low-code applications without customization and compromise.