webinář na vyžádání

Drone noise reduction

Ensure urban air mobility technology adoption using simulation and test

Odhadovaná doba sledování: 49 min

Sdílení

A drone carrying a box and far-field simulation of the noise created by a stationary drone

Drone noise mitigation is a key enabler for urban air mobility technology adoption. Noise pollution is one of the main reasons why helicopter operations are often restricted. Thanks to the distributed electrical propulsion architecture, eVTOL air taxis and drones offer a perspective to reduce sound levels by 15dB at 500ft compared with helicopters.

Achieving this objective is critical to decreasing the overall journey time and thereby increasing the overall attractiveness of this new mobility mode. The challenge at hand is to design disc loading, rotor tip speed, propellor interactions and vehicle scattering in such a way that the overall in-situ noise levels are reduced.

It is a multidisciplinary issue, calling for the combined use of various simulation and testing techniques.

Drone noise

You will learn how to:

  • Combine CFD simulations and acoustic propagation together with raytracing methods to capture drone noise behavior at different scales
  • Model and validate noise sources against physical testing
  • Analyze propellor interactions influence on the noise signature
  • Understand how installation effects of the vehicle influence far-field noise levels
  • Gain insights into the effect of the urban environment on the noise

Drone noise analysis: von Karman Institute for Fluid Dynamics example

A numerical analysis carried out at the von Karman Institute for Fluid Dynamics will be presented dealing with drone tonal noise sources and their near- and far-field propagation patterns. Find out how to:

  • Validate the simulation methodology over a quadcopter against measurements available in the literature
  • Investigate the effects of the rotor-on-rotor interaction, and presence and absence of the body
  • Evaluate the sound scattering effects due to the presence of the drone body

Seznamte se s přednášejícími

von Karman Institute for Fluid Dynamics

Alessandro Zarri

Postdoctoral Researcher, Environmental and Applied Fluid Dynamics Department

Alessandro obtained his master's degree in 2017 from the faculty of aerospace engineering at Politecnico di Torino, Italy. In 2021, he received his PhD at the École Centrale de Lyon, France, with a research work based on aeroacoustics of automotive cooling fans carried out at the von Karman Institute for Fluid Dynamics, Belgium.

Siemens Digital Industries Software

Jens de Boer

Simcenter Solution Manager for Aerospace

Jens is a passionate aerospace engineer. In the past 14 years at Siemens, he collaborated with aerospace companies to adopt and streamline their simulation and test processes throughout the development cycle.

Související zdroje informací

Efektivní správa produktových dat zlepšuje výkonnost v oblasti vývoje výrobků
E-book

Efektivní správa produktových dat zlepšuje výkonnost v oblasti vývoje výrobků

Přečtěte si tuto e-knihu a zjistěte, jaké jsou osvědčené postupy v rámci systému PDM ve společnostech, které se studie zúčastnily. Tyto společnosti se věnují návrhu výrobků, inženýringu a/nebo výrobě.

PLM strategie, která pomáhá plnit požadavky a termíny dodání
E-book

PLM strategie, která pomáhá plnit požadavky a termíny dodání

Průzkum hlavních výzev vedoucích pracovníků v inženýrství – uspokojení požadavků (53 %) a plnění termínů dodání (45 %) – s tím si tato e-kniha ...