Catapult High-Level Synthesis has been successfully employed within NVIDIA for multiple generations of system-on-chip research demonstrations. This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations to identify and fix performance bugs.

Meet the Speaker

NVIDIA Research

Nathaniel Pinckney

Senior Research Scientist

Nate Pinckney received his B.S. degree in engineering from Harvey Mudd College in 2008, and his Ph.D. in electrical engineering from the University of Michigan in 2015. He has authored or coauthored over 40 publications in the areas of high-level synthesis methodologies, low-power VLSI design, and cryptographic accelerators. In 2015, he joined NVIDIA in Austin, TX.

相關資訊

BlueDot:利用 Catapult HLS 加快神經網路型 Deepfield-PQO 的設計速度
White Paper

BlueDot:利用 Catapult HLS 加快神經網路型 Deepfield-PQO 的設計速度

為了要找到最佳的架構,會需要重複的合成並且嘗試多種的輕量化技術,導入 Catapult HLS 簡化此流程,我們能夠透過 HLS 流程快速取得以 FPGA 和 ASIC 為目標的 IP 程式碼。

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th