点播式网络研讨会

Xperi®: A Designer’s Life with HLS

预估观看时长:10 分钟

分享

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection that they know well with RTL for comparison. The second is to use HLS to develop new Neural Network accelerators and how HLS could help them get from algorithm to critical FPGA demonstrators in a time that would not be possible with traditional RTL flow.

This webinar is part 8 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • Customer's experience using HLS for Image Processing and AI
  • Using HLS for algorithms such as Face Detection with RTL for
    comparison
  • How to use HLS to develop new Neural Network accelerators
  • How HLS can help get from algorithm to critical FPGA demonstrators
    faster than with traditional RTL flow

相关资源

飞机制造商使用西门子解决方案来缩短全电动复合材料飞机的产品开发时间
Case Study

飞机制造商使用西门子解决方案来缩短全电动复合材料飞机的产品开发时间

NX、Fibersim 和 Simcenter 提升 Bye Aerospace 的生产力并减少 66% 的工程人员