点播式网络研讨会

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

预估观看时长:22 分钟

分享

STMicroelectronics presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) as well as a method to add constraints to the random values generated in UVMF.

High-Level Synthesis has the great advantage of keeping the design at an algorithmic level, simplifying the translation into RTL. High-Level Verification at C++ level can help to catch several bugs in the earliest stage of the design. The usage of the UVMF (UVM Framework), generated by Catapult, is a good starting point to complete the verification at RTL Level. STMicroelectronics presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) as well as a method to add constraints to the random values generated in UVMF.

主讲嘉宾

Politecnico di Torino

Stefano Moncalvo

MSc Electronic Engineering student

MSc Electronic Engineering student at Politecnico di Torino, specializing in embedded systems. Currently working on the master’s thesis, developing a verification flow for High-Level Synthesis IPs in collaboration with STMicroelectronics.

STMicroelectronics

Martino Zerbini

Digital Design Engineer

Martino Zerbini joined STMicroelectronics in 2006 as Digital Design Engineer. He started using CatapultC in 2010 and introduced its usage inside the Audio Division design team. The main activity was the development of DSP part of Class-D amplifiers. Later he moved inside the MEMS Actuator Division developing laser and micro-mirror drivers. Since 2019, Martino focused his interests on Digital Verification, he is responsible for developing and executing an integrated strategy for the chip verification. From 2021 this includes IPs developed with CatapultC.

相关资源

使用正确的数字工具加速新产品导入
E-book

使用正确的数字工具加速新产品导入

详细了解机器部件和设备制造商目前面临的趋势和挑战,并了解如何以更具成本效益的方式加速将高质量的新产品推向市场。获取电子书。

加快上市时间并提高制造生产力
Infographic

加快上市时间并提高制造生产力

使用数字解决方案更快、更高效、更高质量地推出新产品。在此信息图中了解 Accelerated Product Introduction 解决方案。

平衡新产品的成本、可持续性、质量和速度
E-book

平衡新产品的成本、可持续性、质量和速度

NPI 流程可能既耗时又复杂。获取此电子书,了解企业如何更快、更高效地设计和制造新产品。