点播式网络研讨会

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

预估观看时长:19 分钟

分享

NVIDIA's introductory slide

Catapult High-Level Synthesis has been successfully employed within NVIDIA for multiple generations of system-on-chip research demonstrations. This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations to identify and fix performance bugs.

主讲嘉宾简介

NVIDIA Research

Nathaniel Pinckney

Senior Research Scientist

Nate Pinckney received his B.S. degree in engineering from Harvey Mudd College in 2008, and his Ph.D. in electrical engineering from the University of Michigan in 2015. He has authored or coauthored over 40 publications in the areas of high-level synthesis methodologies, low-power VLSI design, and cryptographic accelerators. In 2015, he joined NVIDIA in Austin, TX.

相关资源

Questa 跨时钟域
Fact Sheet

Questa 跨时钟域

Questa CDC 解决方案仅使用 RTL(和 SDC 约束或 UPF 功耗意图文件),便可自动生成和分析断言,防止出现会导致芯片失效的 CDC 问题。