点播式网络研讨会

From HLS Component to a Working Design

预估观看时长:43 分钟

分享

From HLS Component to a Working Design

Complex algorithms do not exist in a vacuum. After High-Level Synthesis (HLS) is used to create an RTL component, to be useful, it needs to be integrated into a larger system. This means connecting it to other components, a processor, and even software. Once integrated, the system needs to be verified. The verification of the complete environment does not just mean functional correctness, but also needs to consider performance, and in some cases power. This webinar details approaches to integrating accelerator blocks into processor-based sub-systems, interfacing to software, and verifying the accelerator in the context of the larger system. It also covers deploying the system onto a FPGA prototyping board.

This webinar is part 4 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • How HLS is used to implement a computer vision algorithm in either
    an FPGA or ASIC technology and the trade-offs for power and
    performance.
  • How HLS is employed to analyze unique architectures for a very
    energy-efficient inference solution such as a CNN (Convolutional
    Neural Network) from a pre-trained network.
  • How to integrate the design created in HLS into a larger system,
    including peripherals, processor, and software.
  • How to verify the design in the context of the larger system and how
    to deploy it into an FPGA prototype board.

主讲嘉宾简介

Siemens EDA

Russell Klein

HLS Program Director

Russell Klein is a Program Director at Siemens EDA’s (formerly Mentor Graphics) High-Level Synthesis Division focused on processor platforms. He is currently working on algorithm acceleration through the offloading of complex algorithms running as software on embedded CPUs into hardware accelerators using High-Level Synthesis. He has been with Mentor for over 25 years, holding a variety of engineering, marketing and management positions, primarily focused on the boundary between hardware and software. He holds six patents in the area of hardware/software verification and optimization. Prior to joining Mentor he worked for Synopsys, Logic Modeling, and Fairchild Semiconductor.

相关资源

面向重型装备行业的电动车辆转换改造技术
Infographic

面向重型装备行业的电动车辆转换改造技术

重型装备排放法规敦促工程部门将装备转换为高能效的动力系统。了解我们的解决方案。

法国建筑机械制造商使用 Simcenter Amesim 开发电动轮式挖掘机
Case Study

法国建筑机械制造商使用 Simcenter Amesim 开发电动轮式挖掘机

Mecalac 利用 Siemens Digital Industries Software 的解决方案创建一次即成功的原型

在从内燃机转换成电动机的过程中利用仿真技术优化剪式升降机的性能
Case Study

在从内燃机转换成电动机的过程中利用仿真技术优化剪式升降机的性能

Haulotte 采用 Simcenter 将 Pulseo 升降机的上限升降高度提高了 25%,负载容量加大了 50%