High-Level Synthesis (HLS), has been adopted by leading companies to speed design time and reduce verification costs in applications such as video and image processing, 4/5G wireless, and high bandwidth advanced communications designs (i.e. optical communications processors).

But when deciding to use HLS for the first time, designers have many questions:

  • What does high level synthesis code look like for an algorithmic
    block?
  • How do I optimize it, and do I have enough control to get the design
    I want?
  • Will the QoR be good?
  • How do I verify and debug the RTL?
  • Should I use SystemC or C++?

This technical tutorial explores these questions and more using an
iDCT for H.265 as a specific example.

What you will learn:

  • What High-Level Synthesis code look like for an algorithmic block
  • How to optimize HLS code and the level of control in the design
  • What the QoR will look like
  • How to verify and debug the RTL
  • Whether SystemC or C++ should be used

Who should attend:

  • RTL designers interesting in moving up to HLS with C/C++/System
    based design flow to improve productivity
  • RTL Design Manager/Project leaders who want to better understand
    what it will take and the potential benefit for the next project to
    move to HLS
  • Verification Managers who want to understand the design and
    verification flow using HLS

Conteúdo informativo relacionado

Rapid Algorithm to HW: Using HLS for Computer Vision and Deep Learning Seminar
Webinar

Rapid Algorithm to HW: Using HLS for Computer Vision and Deep Learning Seminar

How HLS helps project teams rapidly & accurately explore power/performance of algorithms, quickly get to FPGA implementations to create demonstrator/prototypes & use same source RTL IP for ASIC implementation.

HLS 101 - Fundamentals of High-Level Synthesis
Webinar

HLS 101 - Fundamentals of High-Level Synthesis

High-Level Synthesis (HLS) extends the traditional design flow, providing a new and powerful approach to hardware design. It is important to understan