온디맨드 웨비나

Xperi®: A Designer’s Life with HLS

예상 소요 시간: 10분

공유

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection that they know well with RTL for comparison. The second is to use HLS to develop new Neural Network accelerators and how HLS could help them get from algorithm to critical FPGA demonstrators in a time that would not be possible with traditional RTL flow.

This webinar is part 8 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • Customer's experience using HLS for Image Processing and AI
  • Using HLS for algorithms such as Face Detection with RTL for
    comparison
  • How to use HLS to develop new Neural Network accelerators
  • How HLS can help get from algorithm to critical FPGA demonstrators
    faster than with traditional RTL flow

관련 자료

Siemens 솔루션을 사용하여 순수 전기 복합 항공기의 제품 개발 시간을 단축하는 비행기 제조업체
Case Study

Siemens 솔루션을 사용하여 순수 전기 복합 항공기의 제품 개발 시간을 단축하는 비행기 제조업체

Bye Aerospace는 NX, Fibersim 및 Simcenter를 통해 엔지니어링 직원을 66% 줄여 생산성을 향상합니다