オンデマンド・ウェビナー

Xperi®: A Designer’s Life with HLS

視聴時間の目安: 10 分

共有

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection that they know well with RTL for comparison. The second is to use HLS to develop new Neural Network accelerators and how HLS could help them get from algorithm to critical FPGA demonstrators in a time that would not be possible with traditional RTL flow.

This webinar is part 8 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • Customer's experience using HLS for Image Processing and AI
  • Using HLS for algorithms such as Face Detection with RTL for
    comparison
  • How to use HLS to develop new Neural Network accelerators
  • How HLS can help get from algorithm to critical FPGA demonstrators
    faster than with traditional RTL flow

関連情報

高度なエンジニアリング・シミュレーションによる開発プロセスの改善
Solution Brief

高度なエンジニアリング・シミュレーションによる開発プロセスの改善

開発プロセスを加速して、より良い設計をより迅速に商品化できるようにします。シーメンスの高度なエンジニアリング・シミュレーションが役立ちます。

Role of simulation in the digital twin for energy and process industries
Webinar

Role of simulation in the digital twin for energy and process industries

Physics-based simulation in the digital twin lowers the barrier for executing on the production floor.