オンデマンド・ウェビナー

From HLS Component to a Working Design

おおよその視聴時間43 分

共有

From HLS Component to a Working Design

Complex algorithms do not exist in a vacuum. After High-Level Synthesis (HLS) is used to create an RTL component, to be useful, it needs to be integrated into a larger system. This means connecting it to other components, a processor, and even software. Once integrated, the system needs to be verified. The verification of the complete environment does not just mean functional correctness, but also needs to consider performance, and in some cases power. This webinar details approaches to integrating accelerator blocks into processor-based sub-systems, interfacing to software, and verifying the accelerator in the context of the larger system. It also covers deploying the system onto a FPGA prototyping board.

This webinar is part 4 of the webinar series HLS for Vision and Deep Learning Hardware Accelerators.

What you will learn:

  • How HLS is used to implement a computer vision algorithm in either
    an FPGA or ASIC technology and the trade-offs for power and
    performance.
  • How HLS is employed to analyze unique architectures for a very
    energy-efficient inference solution such as a CNN (Convolutional
    Neural Network) from a pre-trained network.
  • How to integrate the design created in HLS into a larger system,
    including peripherals, processor, and software.
  • How to verify the design in the context of the larger system and how
    to deploy it into an FPGA prototype board.

講演者の紹介

Siemens EDA

Russell Klein

HLS Program Director

Russell Klein is a Program Director at Siemens EDA’s (formerly Mentor Graphics) High-Level Synthesis Division focused on processor platforms. He is currently working on algorithm acceleration through the offloading of complex algorithms running as software on embedded CPUs into hardware accelerators using High-Level Synthesis. He has been with Mentor for over 25 years, holding a variety of engineering, marketing and management positions, primarily focused on the boundary between hardware and software. He holds six patents in the area of hardware/software verification and optimization. Prior to joining Mentor he worked for Synopsys, Logic Modeling, and Fairchild Semiconductor.

関連情報

重機業界向けEV転換のための改造技術
Infographic

重機業界向けEV転換のための改造技術

厳格な規制や絶えず変化する顧客要求によって重機業界は開発プロセスの変革を迫られています。このインフォグラフィックは、EV転換のための改造技術について概説し、機械に最適な電気アーキテクチャの選び方を紹介します。

Simcenter Amesimを使用して電動ホイール式掘削機を初めて開発したフランスの建設機械メーカー
Case Study

Simcenter Amesimを使用して電動ホイール式掘削機を初めて開発したフランスの建設機械メーカー

Mecalacがシーメンスデジタルインダストリーズソフトウェアのソリューションを使用して、初回試作を成功

シミュレーションを活用してシザーリフトの性能を改善し、ICEから電動モーターへと移行
Case Study

シミュレーションを活用してシザーリフトの性能を改善し、ICEから電動モーターへと移行

ハウロッテ、Simcenterを使用して、シザーリフトPulseoの最大揚高を25%、積載荷重を50%改善