オンデマンド・ウェビナー

Enabling MBSE integration with Teamcenter: The key to establishing digital continuity

Realize LIVE | Teamcenter | Cross-industry | Lifecycle management

視聴時間の目安: 17 分

共有

Logo for Realize LIVE, a Siemens Digital Industries Software event for technical users, deployment managers, process leaders and partners
Enabling MBSE integration with Teamcenter: The key to establishing digital continuity

Back to Realize LIVE content library

Organizations in cross-industry are adopting model-based systems engineering (MBSE) approaches to develop efficient, multi-disciplinary product architectures that enable complex use cases and requirements. MBSE tools enable the development of formal models using the Systems Modeling Language (SysML) to capture the structure, interfaces, and interactions, and the allocation of behavior and requirements, etc. However, detailing the design definition for the planned architecture involves manual re-creation of relevant artifacts in domain-specific tools and linking them to maintain traceability. This leads to significant challenges.

HCL has teamed up with Siemens R&D and MBSE tool vendors to develop a unique approach to exchanging architecture artifacts between SysML models and the Teamcenter PLM backbone, breaking barriers between concepting and detailed engineering.

Watch this video for a demonstration of unique features such as single-click exchange of architecture definition, bi-directional synchronization of attributes, parameter integration, seamless handling of reused artifacts, and more. The presentation will also indicate the unique workflows and benefits enabled for the end users by these solutions.

Key takeaways:

  • Understand the Digital Thread and the challenges in enabling it within an organization
  • Learn about HCL’s MBSE-to-PLM connectors
  • Realize benefits of the integration

Who benefits?

  • Aerospace, automotive, medical devices and industrial sectors
  • IT department heads, system architects, engineers
  • Siemens sales, client partners, pre-sales

Back to Realize LIVE content library

講演者の紹介

HCL Technologies Ltd.

Nikhil Joshi

Enterprise architect

関連情報

要件と納期を遵守する最適なPLM戦略
E-book

要件と納期を遵守する最適なPLM戦略

この電子ブックでは、エンジニアリング企業にとっての上位の課題 -- 製品要件への適合 (53%) と納期の遵守 (45%) -- に対応する5つの戦略を説明します。

PLMとは何か。なぜクラウド型PLMなのか。
Infographic

PLMとは何か。なぜクラウド型PLMなのか。

PLMとは何かコスト効果が高く高速のクラウド型Teamcenter Xを導入すると、革新的な製品を市場にいち早く投入できます。その詳細をご覧ください。詳細情報

Teamcenter X SaaS PLMの迅速な導入
Video

Teamcenter X SaaS PLMの迅速な導入

使いやすさとアクセス性に優れたTeamcenter X Software-as-a-Service製品ライフサイクル管理 (SaaS PLM) をぜひお試しください。