Webinar on-demand

High-Level Verification of an AI/ML Accelerator Design

Tempo di visione stimato: 68 minuti

Condividi

This webinar demonstrates how one can achieve comprehensive verification faster at a higher level of abstraction but still apply known and trusted RTL verification techniques.

One of the fastest growing areas of hardware and software design is Artificial Intelligence/Machine Learning (AI/ML), fueled by the demand for more autonomous systems such as computer vision (CV) for self-driving vehicles, voice recognition for personal assistants and many others.  

We are now seeing the emergence of customized AI/ML hardware accelerators to meet numerous, stringent, and potentially conflicting design requirements. High-Level Synthesis (HLS) can provide the needed flexibility and abstraction to efficiently and quickly realize these designs in RTL. However, when working with HLS at the C-level, many have questions about what does verification look like? Waiting to verify until you have post-HLS RTL is too late and too inefficient. This webinar demonstrates how one can achieve comprehensive verification faster at a higher level of abstraction but still apply known and trusted RTL verification techniques. 

Relatori

Siemens EDA

David Aerne

Verification Technologist

Dave Aerne is a Verification Technologist within the Calypto Systems Division, focusing on HLV (High-Level Verification) solutions. His particular areas of expertise are the UVM and Verification IP. Prior to joining the EDA industry, he gained over 18 years of SoC Design and Verification experience in various roles at semiconductor companies and fabless startups. Dave received a BSCompE from the University of Illinois at Urbana-Champaign and a MSCompE from National Technological University in Fort Collins, Colorado.

Siemens EDA

Jonathan Craft

HLS Verification Technologist

Jonathan Craft is an HLS Technologist at Siemens EDA focused on development of High-Level Verification (HLV) tools & methodologies. He holds a Bachelor of Science degree in Electrical Engineering from the University of Wyoming. Prior to working for Siemens, Jon held various design and verification roles performing IC and SoC development at various companies in the Denver, Colorado area.

Risorse correlate

Comfort e sicurezza della cabina nelle attrezzature pesanti
White Paper

Comfort e sicurezza della cabina nelle attrezzature pesanti

Le soluzioni intelligenti di Siemens permettono di migliorare la cabina dei macchinari pesanti, con un impatto positivo sul comfort e la sicurezza dell'operatore, riducendo al contempo i tempi di sviluppo.

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico
Case Study

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico

Haulotte usa Simcenter per aumentare l'altezza massima di lavoro dell'unità di sollevamento Pulseo del 25% e la capacità di carico del 50%

Progettazione ad alte prestazioni con il software di modellazione predittiva
Video

Progettazione ad alte prestazioni con il software di modellazione predittiva

Gestire la complessità meccatronica e migliorare il processo progettuale utilizzando software di modellazione predittiva. Maggiori informazioni