Webinar on-demand

Simulation Process and Data Management (SPDM) for Heavy Equipment

Improve collaboration and efficiency between engineering departments

Tempo di visione stimato: 47 minuti

Condividi

Rendered image of heavy equipment showing two vehicles with innovative technologies and simulation.

Over the past decade, simulation in the heavy equipment industry has exploded to explore new designs while reducing costly prototyping phases. Simulation is used in various engineering domains such as thermal, structural integrity, hydraulics, NVH and more. Consequently, the number of models, analyses, and data has increased considerably.

Watch this on-demand webinar to learn more about how simulation process and data management (SPDM) software aids engineers in predicting product performance while also improving collaboration and efficiency between engineering departments.

MBSE integrated with PLM

By integrating MBSE with PLM you can define what will be built, instruct people how to do it and orchestrate the downstream development process. This creates the critical glue that holds the entire cross-product lifecycle together.

Transparent access to all engineering analyses, using the latest in data models, and smooth interactions and traceably among all engineering departments remains crucial when it comes to the simulation process. Design decision-making must be streamlined to ensure engineering departments save time and money.

Verification management framework

Heavy equipment manufacturers are under increased pressure to develop more complex, integrated machines with compressed delivery times with the expectation of high initial product quality and production rate product costs.  You can achieve both of these objectives with our verification management solution for the heavy equipment industry. This framework enables manufacturers to combine unique capabilities for integrated simulation and test management with plant simulation for manufacturing planning and execution, all while ensuring complete closed-loop requirements traceability.

Teamcenter simulation

Discover how Simcenter solutions can be used in an end-to-end process with a new requirement request for design changes. This is possible through Teamcenter for Simulation (TCSim) which allows a smooth workflow along the program definition.

Learn more about the components of a successful model-based system engineering deployment by registering for this on-demand webinar.

Relatori

Siemens Digital Industry Software

Gaétan Bouzard

Simcenter Heavy Equipment Industry Lead

Siemens Digital Industries Software

Vijay Singh

MBSE Solution Consultant

Singh is an MBSE expert consultant in the industry strategy team of the simulation and test solutions segment. In this role, he is responsible for enabling industry-leading customers to successfully integrate their simulation and test workflows as part of their enterprise MBSE solution.

Risorse correlate

Comfort e sicurezza della cabina nelle attrezzature pesanti
White Paper

Comfort e sicurezza della cabina nelle attrezzature pesanti

Le soluzioni intelligenti di Siemens permettono di migliorare la cabina dei macchinari pesanti, con un impatto positivo sul comfort e la sicurezza dell'operatore, riducendo al contempo i tempi di sviluppo.

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico
Case Study

Utilizzare la simulazione per migliorare le prestazioni di sollevamento a forbice durante la transizione da un motore ICE a un motore elettrico

Haulotte usa Simcenter per aumentare l'altezza massima di lavoro dell'unità di sollevamento Pulseo del 25% e la capacità di carico del 50%

Progettazione ad alte prestazioni con il software di modellazione predittiva
Video

Progettazione ad alte prestazioni con il software di modellazione predittiva

Gestire la complessità meccatronica e migliorare il processo progettuale utilizzando software di modellazione predittiva. Maggiori informazioni