Webinar on-demand

Address e-motor NVH early in electric vehicle development

Skill up the e-motor NVH performance of your electric vehicle

Tempo di visione stimato: 33 minuti

Condividi

Detail of an electric drive with a virtual model used for optimizing e-motor NVH performance.

In hybrid and electric vehicles, passengers often perceive the high-frequency tonal noise of electric motors combined with gearbox whine as annoying. E-drive manufacturers are looking for solutions to address e-motor noise, vibration, and harshness (NVH) early in the development cycle. But the complexity of motor types and configurations makes it difficult to find the perfect trade-off between efficiency and NVH performance.

This on-demand webinar will discuss e-drive solutions both in the early and detailed design stages. The intended audience is e-motor NVH, 3D CAE, and electromagnetic user communities, from experts to analysts, who endeavor to create an e-drive sound and performance that fits their brand.

Gain insights into finding the perfect trade-off between efficiency and NVH

The electric motor development process is challenging; It is repetitive, time-consuming, inflexible. The multiphysics required to reach a robust design relies on collaboration from multiple experts in different fields. Engineers must balance all aspects of development; e-motor design, brand requirements, structural analysis, thermal analysis, and NVH. Siemens' Electrified Vehicle Performance Engineering solution helps teams stay integrated by breaking down silos to enable one environment and workflow for maximum efficiency.

Reduce the risk of e-Drive NVH issues late in the design process

The early stage of e-drive development is where manufacturers make essential design choices for motor and gearbox performance. Part of this early development stage is an early qualitative NVH assessment of the inverter, transmission, and e-motor NVH to understand their impact on overall vehicle performance. This quick and easy evaluation of structural design and inverter control strategy radically reduces the risk of encountering e-drive NVH issues late in the design process.

Predict e-motor noise and identify system sensitivities in the concept phase

Once the electrical parameters of the motor and controls are fixed, engineers can concentrate on more precise prediction of electric motor noise in the detailed design phase. Simulations can be used to analyze the complete system, from electric currents to radiated noise, and integrate electromagnetic, structural, transmission multi-body, and acoustics analysis. The combination of loads and structural/vibro-acoustic model allows engineers to predict the NVH behavior of the e-powertrain. Afterward, the simulation model can evaluate the effect of all possible design modifications.

Watch the on-demand webinar to learn more about the solutions that can boost the NVH performance of your electric drive.

Relatore

Siemens Digital Industries Software

Alessandro Lepore

Business Development Manager

Alessandro has been with Siemens Digital Industries Software for 10 years, working in various roles in the Engineering and Consulting Services division. He is currently Business Development Manager responsible for global business development and go-to-market for Engineering Services Solutions, focusing on technologies that combine Test, 1D, and 3D CAE simulation, the automotive and transportation industry, NVH, acoustics, drivability and, ride and handling solutions.

Risorse correlate

Le migliori strategie PLM per soddisfare i requisiti di prodotto e rispettare i termini di consegna
E-book

Le migliori strategie PLM per soddisfare i requisiti di prodotto e rispettare i termini di consegna

Scopri come le aziende leader dello sviluppo prodotto hanno risolto le principali sfide del settore - Soddisfare i requisiti di prodotto (53%) e rispettare i tempi di consegna (45%) - con le cinque strategie illustrate in ...

Cos'è il PLM e perché scegliere una soluzione PLM in cloud?
Infographic

Cos'è il PLM e perché scegliere una soluzione PLM in cloud?

Cos'è il PLM? Lancia i tuoi prodotti sul mercato in tempi più brevi grazie a Teamcenter X in cloud. Maggiori informazioni.

Teamcenter X: la piattaforma PLM in modalità SaaS
Video

Teamcenter X: la piattaforma PLM in modalità SaaS

Scopri Teamcenter X, la piattaforma per la gestione del ciclo di vita del prodotto (PLM) in modalità cloud SaaS, di facile accesso e utilizzo.