webinaire à la demande

Catapult AI NN – From AI/ML Framework to Optimized RTL

Durée estimée : 13 minutes

Partager

Intro slide to session

As demand for Machine Learning increases, the need for custom hardware acceleration is exploding. Developing hardware that is optimally tuned for Performance, Power & Area (PPA) and optimized to the network and application delivers enormous competitive advantages in silicon. Designers working in AI/ML Frameworks such as TensorFlow, PyTorch have previously relied on “rule of thumb” or RTL design teams to assess the cost of implementation. Catapult AI NN now delivers a methodology and flow from “AI/ML Framework to RTL” enabling rapid exploration of network, quantization, design reuse factors on a layer-by-layer basis for PPA, generating production-ready custom RTL without needing extensive HLS knowledge or RTL skills.

À propos de l'intervenant

Siemens EDA

Stuart Clubb

Technical Product Management Director

Stuart is responsible for Catapult HLS Synthesis and Verification Solutions since July 2017. Prior to this role, Stuart had been successfully managing the North American FAE team for Mentor/Siemens and Calypto Design Systems and was key to the growth achieved for the CSD products after the Calypto acquisition. Moving from the UK in 2001 to work at Mentor Graphics, Stuart held the position of Technical Marketing Engineer, initially on the Precision RTL synthesis product for 6 years and later on Catapult for 5 years. He has held various engineering and application engineering roles ASIC and FPGA RTL hardware design and verification. Stuart graduated from Brunel University, London, with a Bachelors of Science.

Ressources associées

Utilisation de l'ingénierie des systèmes basée sur des modèles pour développer un jumeau numérique complet des fonctionnalités ADAS
Case Study

Utilisation de l'ingénierie des systèmes basée sur des modèles pour développer un jumeau numérique complet des fonctionnalités ADAS

Utilisation de l'ingénierie des systèmes basée sur des modèles pour développer un jumeau numérique complet des fonctionnalités ADAS

Validation et vérification de la simulation de capteurs basée sur la physique
Webinar

Validation et vérification de la simulation de capteurs basée sur la physique

Vérification et validation complètes de la simulation de capteurs basée sur la physique automobile pendant le développement en modélisant un environnement de jumeau numérique. En savoir plus