webinar a la carta

INOVA Semiconductors and Coseda: Paradigm Shift in Mixed Signal ASIC Design, Adopting SystemC and High-Level-Synthesis vs. Traditional RTL Design Flow

Tiempo estimado de visualización: 29 minutos

Compartir

Title slide from the session: Paradigm Shift in Mixed Signal ASIC Design, Adopting SystemC and High-Level-Synthesis vs. Traditional RTL Design Flow

The authors present the adoption of SystemC for High-Level-Synthesis replacing the traditional RTL design flow. A steady increase in the need for connectivity in the automotive industry and the resulting higher complexity in the individual ASICs requires a novel methodology within the ASIC design phase. This is now being implemented using a new design flow starting from an abstract network simulation in SystemC down to either FPGA-Prototyping (simulating a complex network topology) or the tapeout RTL for an individual ASIC. In conclusion, the authors will present the ease of use and the value-add of the HLS methodology in an automotive context.

Conoce a los ponentes

INOVA Semiconductors

Fabian Kluge

Systems Engineering Manager

Fabian Kluge is a Systems Engineering Manager at INOVA Semiconductors, working on architectures and concepts for new automotive serializers and networking products, now adopting SystemC as a modelling language. He has a strong background in FPGA and general electronics development including various high-speed interfaces. He received his master’s degree in electrical engineering from Technical University Munich in 2017, specializing in EDA and radar technologies.

Coseda

Thomas Arnt

Application Engineering Manager

Thomas Arndt is an Application Manager at COSEDA Technologies, focusing on system level design and simulation solutions. He has over 20 years of experience in the chip design and the EDA industry. His particular areas of expertise are in the field of digital as well as analog system design, simulation and High-Level Synthesis. Prior to joining COSEDA, he was working at the Fraunhofer Institute for Integrated Circuits, one of the largest research institutions in the field of design automation in Europe. He received his diploma in electrical engineering from the Technical University of Dresden.

Recursos relacionados

El proceso del diseñador del concepto a la fabricación
Infographic

El proceso del diseñador del concepto a la fabricación

Desde el concepto hasta la fabricación, descubre los cuatro pasos completos que efectúan los diseñadores con Siemens Digital Industries Software.

Informe del empresario sobre la ingeniería acelerada y la transformación digital
Webinar

Informe del empresario sobre la ingeniería acelerada y la transformación digital

Ve este webinar para saber más sobre la transformación digital de las pequeñas y medianas empresas y los retos a los que se enfrentan a partir de una encuesta llevada a cabo por Lifecycle Insights.

Estudio de estrategias de ingeniería para pymes 2022
E-book

Estudio de estrategias de ingeniería para pymes 2022

Formula estrategias exitosas para mejorar la ingeniería y cambiar hacia un futuro rentable. Este estudio proporciona información detallada sobre estrategias de ingeniería para pymes en 2022.