webinar a la carta

Faster time to market in pharmaceutical industry

Tiempo estimado de visualización: 42 minutos

Compartir

Women working in pharmaceutical industry

Within the pharmaceutical industry, there is a constant drive for innovation and faster time to market, looking to develop new processes, improve the efficiency of existing processes, and quickly move from lab scale to demonstration and commercial scale. When transferring processes between scales, most businesses will need to use an intermediate scale, which may not be perfectly aligned with either the lab-scale process or the envisioned commercial-scale equipment.

Pharmaceutical modelling

To design the most time and cost-efficient production processes, teams around the world leverage computer-aided engineering (CAE) using innovative methods. The key in the scale-up process is to define the effect of the operating parameters and get a deep understanding of their effects. You need to consider the limitations imposed upon you by the process equipment with which you are developing your process. This is where implementing computational fluid dynamics (CFD) and discrete element method (DEM) plays an essential role in pharmaceutical modeling.

Process design in pharmaceutical industry

This is the path the Centre for Process Innovation (CPI) selected to define areas for special attention in process and equipment design, leading to a faster transition to commercial scale.

In this webinar, Kristi Potter and Alex Smith from CPI will present two use cases related to granular powder flow and developing a soft sensor using CFD simulation. Both cases show that modeling can be used to identify and remedy limitations in process equipment that can be used for pharmaceutical applications and a range of other industries.

Learn how CFD simulation and discrete element modeling capability enable companies to validate the appropriateness of new designs prior to fabrication.

Pharmaceutical process engineering

Some of the factors affecting process scale-up along with some of the modeling approaches used to provide insight into the limitations inherent within process equipment include:

  • The key considerations of scale-up on equipment geometry
  • Effects of process equipment geometry on powder flow       
  • Meshing techniques used to model complex motions in equipment simulations
  • The use of simulation operations to automate tasks
  • Identification of the source of unexpected experimental results in a
    test rig

Register to watch this webinar and learn more about the value and results achieved by implementing the DEM methodology demonstrated in actual use cases

Conoce a los ponentes

CPI - The Centre for Process Innovation

Alex Smith

Head of Process Safety & Engineering

CPI - The Centre for Process Innovation

Kristi Potter

Process Engineer

Siemens Digital Industries

Glenn Longwell

Portfolio Development Executive

Glenn Longwell is responsible for the implementation of the physics based simulation portfolio (Simcenter) in the Pharmaceutical and CPG markets in the U.S. With a BS in Chemical Engineering, Glenn has over 37+ years in the Computer Aided Engineering (CAE) space helping companies implement and gain value from simulation.

Recursos relacionados

Descubra mejores diseños rápidamente: Simulación multidisciplinar y exploración del diseño en la industria química y de procesos
White Paper

Descubra mejores diseños rápidamente: Simulación multidisciplinar y exploración del diseño en la industria química y de procesos

Lea este informe especial para comprobar cómo las empresas en el sector químico y de procesos están implementando la simulación CFD para predecir ...

Desarrollo de una estructura para analizar el rendimiento de un reactor térmico con CFD
White Paper

Desarrollo de una estructura para analizar el rendimiento de un reactor térmico con CFD

Porter McGuffie utiliza Simcenter STAR-CCM+ para desarrollar una estructura que analiza el rendimiento del reactor térmico con CFD