on-demand webinar

Vias and Stackups

Estimated Watching Time: 60 minutes

Share

via and stackup

As signaling speeds continue to increase, via design and planning are becoming a significant part of the process of designing for signal integrity.

We all want simulators that can model detailed electromagnetic behavior and produce highly accurate results, but what happens if you build something different than what you simulated? While no one does that deliberately, the fact is – it happens all the time because the details of the materials and processes used to build the board aren’t accurately represented in the simulation model.

As speeds go faster and margins get smaller, the small details of board fabrication – like plating layer thickness, or metal roughness on core vs. prepreg vs. plating surfaces – can significantly impact design performance. In order to ensure simulation results are accurate, it has become critical to model and analyze a board as it will be manufactured – instead of using traditional methods.

This webinar will show you how to evaluate PCB tradeoffs and create a detailed board model that ensures that the detailed design simulations you perform reflect the behavior of the board as it will actually be built, instead of reflecting the behavior of a board as you wish it could be built.

What you will learn:

  • How via planning impacts signal integrity
  • Via planning as part of the stackup design process
  • Vias in the PCB fabrication process
  • Via types and construction requirements
  • How to ensure your PCB stackup is real, before running simulations

Who should attend:

  • SI & PI specialists looking to make their simulations more accurate
  • Hardware system designers looking to accelerate their design's transition into manufacturing
  • New Product Introduction (NPI) engineers working with PCB fabricators
  • Hardware design managers looking to improve the interface between design & manufacturing

Meet the speaker

Z-zero

Bill Hargin

CEO

Bill Hargin is the chief everything officer at Z-zero, developer of the PCB stackup design and material selection software, Z-planner Enterprise. Bill is an industry pioneer, with more than 25 years working in PCB signal integrity and manufacturing, while authoring dozens of articles on signal integrity, stackup design, and material selection. Hargin is also the author of the iConnect007 publication Stackups, the Design within the Design, a regular columnist for Printed Circuit Design and Fabrication magazine, and a contributing author for the Printed Circuits Handbook.

Bill is a regular speaker and panelist at both DesignCon and PCB West, and more than 10,000 engineers and PCB designers worldwide have taken his workshop on high-speed PCB design. Mr. Hargin served as director of marketing for Mentor Graphics’ HyperLynx SI software and as the Director of North American Marketing for Nan Ya Plastic’s PCB laminate division in Taiwan before founding Z-zero.

Related resources

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP
Webinar

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

STMicro presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) and a method to add constraints to the random values generated in UVMF.

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?
Webinar

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?

Discover how C++ & SystemC/MatchLib HLS is more than just converting SystemC to RTL. In the RTL Design space, we will cover our technology for Power Optimization with PowerPro Designer & Optimizer.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm
Webinar

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm

Space Codesign Seminar: design flow including HW/SW co-design & HLS that allows developers to migrate compute intensive functions from software running on an embedded processor to a hardware based accelerator.