on-demand webinar

Drone noise reduction

Ensure urban air mobility technology adoption using simulation and test

Estimated Watching Time: 49 minutes

Share

A drone carrying a box and far-field simulation of the noise created by a stationary drone

Drone noise mitigation is a key enabler for urban air mobility technology adoption. Noise pollution is one of the main reasons why helicopter operations are often restricted. Thanks to the distributed electrical propulsion architecture, eVTOL air taxis and drones offer a perspective to reduce sound levels by 15dB at 500ft compared with helicopters.

Achieving this objective is critical to decreasing the overall journey time and thereby increasing the overall attractiveness of this new mobility mode. The challenge at hand is to design disc loading, rotor tip speed, propellor interactions and vehicle scattering in such a way that the overall in-situ noise levels are reduced.

It is a multidisciplinary issue, calling for the combined use of various simulation and testing techniques.

Drone noise

You will learn how to:

  • Combine CFD simulations and acoustic propagation together with raytracing methods to capture drone noise behavior at different scales
  • Model and validate noise sources against physical testing
  • Analyze propellor interactions influence on the noise signature
  • Understand how installation effects of the vehicle influence far-field noise levels
  • Gain insights into the effect of the urban environment on the noise

Drone noise analysis: von Karman Institute for Fluid Dynamics example

A numerical analysis carried out at the von Karman Institute for Fluid Dynamics will be presented dealing with drone tonal noise sources and their near- and far-field propagation patterns. Find out how to:

  • Validate the simulation methodology over a quadcopter against measurements available in the literature
  • Investigate the effects of the rotor-on-rotor interaction, and presence and absence of the body
  • Evaluate the sound scattering effects due to the presence of the drone body

Meet the speakers

von Karman Institute for Fluid Dynamics

Alessandro Zarri

Postdoctoral Researcher, Environmental and Applied Fluid Dynamics Department

Alessandro obtained his master's degree in 2017 from the faculty of aerospace engineering at Politecnico di Torino, Italy. In 2021, he received his PhD at the École Centrale de Lyon, France, with a research work based on aeroacoustics of automotive cooling fans carried out at the von Karman Institute for Fluid Dynamics, Belgium.

Siemens Digital Industries Software

Jens de Boer

Simcenter Solution Manager for Aerospace

Jens is a passionate aerospace engineer. In the past 14 years at Siemens, he collaborated with aerospace companies to adopt and streamline their simulation and test processes throughout the development cycle.

Related resources

LG Electronics: Video Encoder IP Design Optimization and Verification Using Catapult
Webinar

LG Electronics: Video Encoder IP Design Optimization and Verification Using Catapult

In this session, LGE describes a new design approach which concluded that adopting Catapult in IP development increases efficiency in time and cost, and they plan to increase usage in future IP projects.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.

Catapult AI NN – From AI/ML Framework to Optimized RTL
Webinar

Catapult AI NN – From AI/ML Framework to Optimized RTL

Video describing how Catapult AI NN now delivers a methodology and flow from “AI/ML Framework to RTL” enabling rapid exploration of network, quantization, design reuse factors, and more!

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

Hardware Accelerators – Exploring Power and Performancein Today’s AI
Webinar

Hardware Accelerators – Exploring Power and Performance in Today’s AI

This session explores the design process from algorithm to hardware accelerator on a RISC-V processor as we quantify power consumption and performance.

Nokia: Experience in Adopting HLS and HLV Methodology
Webinar

Nokia: Experience in Adopting HLS and HLV Methodology

For increasing requirements for shorter time to market, Nokia has explored is raising abstraction level in both RTL design and verification with the help of High-Level Synthesis and Verification tools.

STMicroelectronics: In sensor Bricks Multi-objective Optimization of an Algorithm Chain for In-Sensor Processing
Webinar

STMicroelectronics: In sensor Bricks Multi-objective Optimization of an Algorithm Chain for In-Sensor Processing

Through HLS and their innovative modular system, STMicroelectronics leads in the seamless integration of digital intelligence into analog native products, setting new standards for efficiency and market.

INOVA Semiconductors and Coseda: Paradigm Shift in Mixed Signal ASIC Design, Adopting SystemC and High-Level-Synthesis vs. Traditional RTL Design Flow
Webinar

INOVA Semiconductors and Coseda: Paradigm Shift in Mixed Signal ASIC Design, Adopting SystemC and High-Level-Synthesis vs. Traditional RTL Design Flow

The authors will present the ease of use and the value-add of the HLS methodology in an automotive context.

HW Acceleration with High-Level Synthesis
Webinar

HW Acceleration with High-Level Synthesis

Session introduces High-Level Synthesis, a technology that allows a developer to take a C++ function and automatically compile it into an RTL hardware description, suitable to be deployed into an ASIC or FPGA.

Fermilab: Bridging Machine Learning and Hardware Design with hls4ml and Catapult HLS
Webinar

Fermilab: Bridging Machine Learning and Hardware Design with hls4ml and Catapult HLS

Fermilab introduces their partnership with Siemens to provide full integration with Catapult HLS design & verification flow, describe projects that have benefitted from hls4ml, and outline future directions.

Oak Ridge National Lab (ORNL): A Spiking Neural Network Architecture for Ultra-low Power and Ultra-low Latency Computing
Webinar

Oak Ridge National Lab (ORNL): A Spiking Neural Network Architecture for Ultra-low Power and Ultra-low Latency Computing

ORNL with the help of the Siemens EDA tools, including Catapult HLS, the neuromorphic accelerator is being adapted from an FPGA prototype to a more capable and lower-power ASIC implementation.

How NVIDIA Uses High-Level Synthesis Tools for AI Hardware Accelerator Research
Webinar

How NVIDIA Uses High-Level Synthesis Tools for AI Hardware Accelerator Research

With constant change in AI/ML workloads, NVIDIA leverages a High-Level Synthesis design methodology based off SystemC and libraries like MatchLib to maximizing code reuse & minimizing design verification effort

Telechips: RTL Hardware Design Acceleration for On-The-Fly Image (De-)Warper in Automotive SoC Using C++ HLS
Webinar

Telechips: RTL Hardware Design Acceleration for On-The-Fly Image (De-)Warper in Automotive SoC Using C++ HLS

Telechips designed a new dewarping engine processing video stream data on-the-fly, different from traditional GPU-based memory-to-memory approach, by utilizing hierarchical design methodology in Catapult HLS.

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP
Webinar

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

STMicro presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) and a method to add constraints to the random values generated in UVMF.

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?
Webinar

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?

Discover how C++ & SystemC/MatchLib HLS is more than just converting SystemC to RTL. In the RTL Design space, we will cover our technology for Power Optimization with PowerPro Designer & Optimizer.

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis
Webinar

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis

Infineon & Coseda present on the adoption of High-Level-Synthesis at an existing SystemC system level model.

Ultra Video Group (Tampere University): Managing the Complexity of an HEVC Encoder (Kvazaar) Implementation on FPGA with Catapult HLS
Webinar

Ultra Video Group (Tampere University): Managing the Complexity of an HEVC Encoder (Kvazaar) Implementation on FPGA with Catapult HLS

Dr. Panu Sjövall from Ultra Video Group (Tampere University), sheds light on how they were able to implement their embedded real-time HEVC intra encoder (Kvazaar) on HW with Catapult HLS.

Quantization of HLS Designs Using Value Range Analysis
Webinar

Quantization of HLS Designs Using Value Range Analysis

Introduces simple & robust quantization methodology based on value range analysis. Learn what’s fixed-point conversion a.k.a quantization; dynamic & static quantization methods; and how to use Catapult VRA.

DUTh: Architectural Improvements for Low-Power and Functional Safety of Dataflow CNN Accelerators Using HLS
Webinar

DUTh: Architectural Improvements for Low-Power and Functional Safety of Dataflow CNN Accelerators Using HLS

DUTh demos using HLS to design CNN accelerators with on-line checking capabilities, improve power efficiency due to optimized data handling on spatial variants of convolution, and effectively use HLS.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.

Cornell University: Building Sparse Linear Algebra Accelerators with HLS
Webinar

Cornell University: Building Sparse Linear Algebra Accelerators with HLS

Cornell intros HiSparse: accelerator on sparse-matrix dense-vector multiplication. Using both HLS implementation and simulation, their sparse accelerators deliver promising speedup.

FNAL: Ultrafast Neural Networks for On-Detector Edge Processing in Resource-Constrained Extreme Radiation Environment
Webinar

FNAL: Ultrafast Neural Networks for On-Detector Edge Processing in Resource-Constrained Extreme Radiation Environment

FNAL demos that a NN autoencoder model can be implemented in a radiation-tolerant ASIC to perform lossy data compression. This alleviates the data transmission problem.

Harvard University: Effective SW/HW Co-Design of Specialized ML Accelerators Using Catapult HLS
Webinar

Harvard University: Effective SW/HW Co-Design of Specialized ML Accelerators Using Catapult HLS

Harvard sheds light on their agile algo-hw co-design & co-verification methodology powered by HLS. It led to an order of magnitude improvement in the design effort across 3 generations edge AI accelerator SoCs.

Stanford University: Edge ML Accelerator SoC Design Using Catapult HLS
Webinar

Stanford University: Edge ML Accelerator SoC Design Using Catapult HLS

Describes the design and verification of the systolic array-based DNN accelerator taped out by Stanford, the performance optimizations of the accelerator, and the integration of the accelerator into an SoC.

From Simulink to High-Quality RTL using High-Level Synthesis - The Design Methodology
Webinar

From Simulink to High-Quality RTL using High-Level Synthesis - The Design Methodology

Webinar introducing a design methodology starting from a flat floating-point Simulink model and step through to HLS generated RTL. All design steps including fixed-point conversion are described in detail.

From MATLAB® to High-Quality RTL Using High-Level Synthesis - The Design Methodology
Webinar

From MATLAB® to High-Quality RTL Using High-Level Synthesis - The Design Methodology

Webinar introducing a design methodology that starts from a self-contained MATLAB script and goes through the different workflow steps to HLS generated, high-quality RTL. All design steps are detailed.

High-Level Verification of an AI/ML Accelerator Design
Webinar

High-Level Verification of an AI/ML Accelerator Design

This webinar demonstrates how one can achieve comprehensive verification faster at a higher level of abstraction but still apply known and trusted RTL verification techniques.

HLS 101 - What Every RTL HW Design Team Needs to Know
Webinar

HLS 101 - What Every RTL HW Design Team Needs to Know

High-Level Synthesis (HLS) extends the traditional design flow, providing a new and powerful approach to hardware design. It is important to understan

Microsoft - HLS Hardware Design Patterns
Webinar

Microsoft - HLS Hardware Design Patterns

High-Level Synthesis (HLS) using untimed C++ presents an elegant hardware abstraction framework for simplifying hardware design at the unit level. To

 Doing Research with Catapult HLS at Harvard
Webinar

Doing Research with Catapult HLS at Harvard

One of them is about proposing adaptive floating-point (FP) quantization to replace integer (INT) quantization for NNs.

NVIDIA: Design and Verification of a Machine Learning Accelerator SoC Using an Object-Oriented HLS-Based Design Flow
Webinar

NVIDIA: Design and Verification of a Machine Learning Accelerator SoC Using an Object-Oriented HLS-Based Design Flow

A high-productivity digital VLSI flow for designing complex SoCs is presented in this webinar. It includes High-Level Synthesis tools, an efficient im

Leveraging HLS IP to Accelerate Design and Verification
Webinar

Leveraging HLS IP to Accelerate Design and Verification

Webinar about how leveraging HLS IP and reference designs to accelerate AI and Image/Signal Processing.

Porting Vivado HLS Designs to Catapult HLS Platform
Webinar

Porting Vivado HLS Designs to Catapult HLS Platform

This webinar will cover how to port an existing HLS design developed within the Xilinx® Vivado® HLS environment into Siemens' Catapult® HLS Platform.

Early AXI4 SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS
Webinar

Early AXI4 SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS

This webinar will introduce NVIDIA Matchlib and its usage with Catapult HLS using some AXI4 SOC demonstration examples.

From HLS Component to a Working Design
Webinar

From HLS Component to a Working Design

Complex algorithms do not exist in a vacuum. After High-Level Synthesis (HLS) is used to create an RTL component, to be useful, it needs to be integra

Part 1: Why Are High-Performance Low-Energy Applications Moving from GPUs and DSPs to FPGAs and ASICs?
Webinar

Part 1: Why Are High-Performance Low-Energy Applications Moving from GPUs and DSPs to FPGAs and ASICs?

Transistor counts and performance of integrated circuits are reaching their peak. Artificial intelligence is emerging as the next "big thing" in areas

Part 2: Adapting software algorithms to hardware architectures for high performance and low-power
Webinar

Part 2: Adapting software algorithms to hardware architectures for high performance and low-power

GPUs and DSPs offer very high-parallelism and impressive memory bandwidths, within the scope of a fully programmable platform. However, they need to f

High-Level Verification: Verification Methodology and Flows When Using C++ and HLS
Webinar

High-Level Verification: Verification Methodology and Flows When Using C++ and HLS

Highlights proven tools and methodology that help an HLS designer check and verify his design, measure, and close coverage, and compare the C to RTL implementation.

Building an iDCT for H.265 Using High-Level Synthesis
Webinar

Building an iDCT for H.265 Using High-Level Synthesis

High-Level Synthesis (HLS), has been adopted by leading companies to speed design time and reduce verification costs in applications such as video and

Catapult HLS for RTL Teams - What You Need to Know
Webinar

Catapult HLS for RTL Teams - What You Need to Know

Catapult® HLS is a key competitive technology in several emerging markets like machine learning and vision. In this webinar, we cover both an introduc

Implementing Machine Learning Hardware Using High-Level Synthesis
Webinar

Implementing Machine Learning Hardware Using High-Level Synthesis

Neural networks are typically developed and trained in a high-performance 32-bit floating-point compute environment. But, in many cases a custom hardw

Using high-level synthesis to accelerate computer/machine Vision applications
Webinar

Using high-level synthesis to accelerate computer/machine Vision applications

High-Level Synthesis (HLS) has been used in multiple companies, projects, and designs targeting vision processing for the past several years. HLS adop

Using HLS to Accelerate Computer Vision for Autonomous Drive
Webinar

Using HLS to Accelerate Computer Vision for Autonomous Drive

The algorithms to teach a computer to see, understand and make decisions for ADAS and Autonomous Drive systems require a significant amount of paralle

Stanford/AMD: Automated Methodology for Efficient Hardware Accelerator
Webinar

Stanford/AMD: Automated Methodology for Efficient Hardware Accelerator

Mobile devices today are composed of many specialized accelerators to achieve high-performance and low-power specifications. However, accelerator desi

Machine Learning: How HLS Can Be Used to Quickly Create FPGA/ASIC HW for a Neural Network Inference Solution
Webinar

Machine Learning: How HLS Can Be Used to Quickly Create FPGA/ASIC HW for a Neural Network Inference Solution

This session reviews the consideration around fast HW prototyping for validating acceleration in Neural Networks for Inferencing vs highest performance implementation and the tradeoffs.

Neural Network Quantization for Low-Power
Webinar

Neural Network Quantization for Low-Power

This webinar will describe how to use Qkeras and High-Level Synthesis to produce a bespoke quantized CNN accelerator, and compares the accuracy, power, performance, and area of different quantizations.

Moving Between FPGA and ASIC with High-Level Synthesis
Webinar

Moving Between FPGA and ASIC with High-Level Synthesis

Writing RTL that works smoothly on both FPGA and ASIC implementations is nearly impossible. But, High-Level Synthesis (HLS) can make technology-indepe

Solutions for the Design and Verification of 5G SoCs
Webinar

Solutions for the Design and Verification of 5G SoCs

Catapult, Veloce 5G Fronthaul, Veloce X-STEP, Questa