On-Demand-Webinar

Machine Learning: How HLS Can Be Used to Quickly Create FPGA/ASIC HW for a Neural Network Inference Solution

Geschätzte Wiedergabezeit 53 Minuten

Teilen

Machine Learning: How HLS Can Be Used to Quickly Create FPGA/ASIC HW for a Neural Network Inference Solution

HLS (High-Level Synthesis) has the unique ability to go from complex algorithms written in C to RTL enabling accurate profiles for power and performance for an algorithm's implementation without having to write it by hand. Neural Networks are typically developed and trained in a high-performance compute environment but in many cases, the inference solution can be reduced and then HW accelerators are the only solution to meet power and real-time requirements. This session reviews the consideration around fast HW prototyping for validating acceleration in Neural Networks for Inferencing vs highest performance implementation and the tradeoffs.

This webinar is part 4 of the seminar Rapid Algorithm to HW: Using HLS for Computer Vision and Deep Learning.

What you will learn:

  • How HLS can be used to implement an example Computer Vision
    Algorithm in either an FPGA or ASIC technology and the trade-offs for
    power and performance. You will walk away with examples, building
    blocks, etc that are completed and can be referenced.
  • How to achieve faster but complete verification signoff in an HLS
    flow measuring quality, coverage; saving days and weeks in
    verification costs
  • How HLS can be applied in multiple ways to implement acceleration
    for Deep Learning and in particular Convolutional Neural Networks. You
    will walk away with examples, building blocks, etc that are completed
    and can be referenced.

Who should view:

  • RTL Designers or Project Managers interested in moving up to HLS
  • Architects or Algorithm developers in the field of image processing,
    computer vision, machine and deep learning interested in rapid and
    accurate exploration of power/performance metrics
  • New Project teams with only a few designers and multiple SW experts
    wanting to rapidly create high-performance FPGA or ASIC IP for
    Computer Vision or Deep Learning markets

Vorstellung des Referenten

Siemens EDA

Michael Fingeroff

HLS Technologist

Michael Fingeroff has worked as an HLS Technologist for the Catapult High-Level Synthesis Platform at Siemens Digital Industries Software since 2002. His areas of interest include Machine Learning, DSP, and high-performance video hardware. Prior to working for Siemens Digital Industries Software, he worked as a hardware design engineer developing real-time broadband video systems. Mike Fingeroff received both his bachelor's and master's degrees in electrical engineering from Temple University in 1990 and 1995 respectively.

Verwandte Ressourcen

Strategien für die Zeitersparnis bei der CAD-Konstruktion mit einem besseren Produktdatenmanagement
E-book

Strategien für die Zeitersparnis bei der CAD-Konstruktion mit einem besseren Produktdatenmanagement

Lernen Sie die besten CAD-Datenmanagement-Strategien kennen, um die fünf größten Zeitfresser zu vermeiden. Laden Sie das kostenlose E-Book des Marktforschungsunternehmens Tech-Clarity herunter, um mehr darüber zu erfahren.

Was ist PLM, und warum PLM in der Cloud?
Infographic

Was ist PLM, und warum PLM in der Cloud?

Was ist PLM? Erfahren Sie, wie Sie mit dem schnellen und kostengünstigen Teamcenter X in der Cloud innovative Produkte schneller auf den Markt bringen können. Erfahren Sie mehr.