On-Demand-Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

Geschätzte Wiedergabezeit: 31 Minuten

Teilen

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc. HLS tools are expected to synthesize this code to RTL which can be input to the traditional RTL downstream flow (RTL / GDS) RTL lint / formal check tools cannot be run on HLS RTL (as the errors cannot be correlated to HLS source code) Onespin systemC/C++ extension DV help to overcome this challenge. This session will be presented by Siemens on behalf of Infineon Technologies AG.

Vorstellung des Referenten

Siemens EDA

Vlada Kalinic

SystemC Product Specialist

Vlada Kalinic is the SystemC Product Specialist at Siemens EDA, and is involved in the evaluations with the new customers as well supporting the current portfolio of the customers to improve the current SystemC flows. Vlada has also another role, as Product Specialist of EC-FPGA in OneSpin. Vlada holds a master’s degree with honors in Electrical and Computer Engineering, Embedded Systems and Algorithms from the University of Novi Sad (Serbia). Prior to Mentor/Siemens, Vlada worked with OneSpin for 5+ years and was involved in various successful evaluations with SystemC and EC-FPGA customers.

Verwandte Ressourcen

Beschleunigung der Innovation im Konsumgüterbereich durch Verbraucherorientierung
Webinar

Beschleunigung der Innovation im Konsumgüterbereich durch Verbraucherorientierung

Mit Siemens und Accenture können Sie die Transformation in der Konsumgüterindustrie erfolgreich meistern.

Revolutionierung der Konsumgüterindustrie: Die innovative Lösung von Siemens & Accenture
White Paper

Revolutionierung der Konsumgüterindustrie: Die innovative Lösung von Siemens & Accenture

Erfahren Sie, wie die innovative cloudbasierte Lösung von Siemens und Accenture die Produktentwicklung in der Konsumgüterindustrie revolutioniert.