webinář na vyžádání

Validation and verification of physics-based sensor simulation

Physics-based sensor simulation supports road safety and comfort

Odhadovaná doba sledování: 35 min

Sdílení

Physics-based sensor simulation, verification, and validation for autonomous vehicles

High-fidelity sensor simulation is required to develop and test autonomous vehicles thoroughly. Simcenter Prescan is a leading simulation platform for testing and developing autonomous vehicle functionality. The physics-based sensor simulations of Simcenter Prescan provide the highest level of detail and are state-of-the-art in the market. However, are the quality and correctness of those high-fidelity sensor models ensured?

This webinar will discuss our approach to verification and validation of automotive sensor simulation, including the following topics:

  • Verification during development of the simulation
  • ISO26262 certification of the software
  • Verification and validation (V&V) of the simulation through dedicated projects

Model a digital twin of the environment of the sensor in simulation

Three key components are essential to provide an excellent physics-based simulation. Physical devices provide sensor-specific highway configuration, physical properties, noise, and patterns, while the simulation engine handles effects such as bounces (ray tracing), energy returns, and weather. The world component consists of a digital twin containing the geometry of 3D models, materials (measured, validated), and environment. By using a digital twin of the vehicle, engineers can design and test vehicle control algorithms to identify system performance under challenging conditions, find system boundaries and solve critical issues early.

Reproduce physics-based sensor effects in simulation with Simcenter Prescan

Simcenter Prescan is the core simulation engine for environments, scenarios, sensors, AI, and controllers, and its representations contain the reflective properties for radar, camera, lidar, and ultrasonic sensors. Simcenter Prescan allows the reproduction of camera effects in simulation, including different fidelity outputs, reflection, weather and light effects, physical device, micro-doppler of wheels, ghost target detection, and doppler ambiguity. It also allows for Lidar effects reproduced in simulation, such as motion distortion, multi bounce, and physics-based material reflections. These sensor models can be scaled from basic ground truth information to full-wave propagation modeling for detailed sensor evaluations.

Verification and validation of sensor simulation during development

Automakers will have to prove the thoroughness of their development processes and robustness of the vehicle’s automated driving systems for occupant safety. Because of this, automated driving systems will have to react safely to all possible traffic scenarios under any likely weather and road conditions. However, the technology enabling this is complex and requires a validation and verification process that allows performance testing in a large number of circumstances. Fortunately, Simcenter Prescan can reproduce crucial real-world effects that affect system performance, allowing for accurate simulation validated against real-world measurements.

Watch the on-demand webinar to learn more about our physics-based sensor simulation solutions for autonomous vehicle development.

Seznamte se s přednášejícím

Siemens Digital Industries Software

Bart Heijke

Product Manager Software and Services

Související zdroje informací

Pokročilá strojírenská výroba - využití PLM ke zlepšení vývoje strojů a průmyslových výrobků
White Paper

Pokročilá strojírenská výroba - využití PLM ke zlepšení vývoje strojů a průmyslových výrobků

Tento dokument obsahuje přehled výhod řešení pokročilého strojírenství společnosti Siemens PLM Software (Siemens PLM), které přináší mj. snadnou implementaci změn návrhů během vývoje výrobků.

Integrovaný přístup k návrhu strojů, správě projektů a konfiguraci
E-book

Integrovaný přístup k návrhu strojů, správě projektů a konfiguraci

Buďte o krok napřed před globální konkurencí a zajistěte si prostředí, které bude zaměstnance motivovat v práci na výzvách. Zjistěte o tomto řešení více.