webinář na vyžádání

Early AXI4 SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS

Odhadovaná doba sledování: 24 min

Sdílení

Early AXI SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS

NVIDIA Matchlib is a new open source library that enables much faster design and verification of SOCs using High-Level Synthesis (HLS). One of the primary objectives of Matchlib is to enable performance accurate modeling of SOCs in SystemC/C++. With these models, designers can identify and resolve issues such as bus and memory contention, arbitration strategies, and optimal AXI4 interconnect structure at a much higher level of abstraction than RTL. In addition, much of the system level verification of the SOC can occur in SystemC/C++, before RTL is even created. Once the architectural performance is verified, this flow provides a fully automated flow to silicon using Catapult HLS. This webinar will introduce NVIDIA Matchlib and its usage with Catapult HLS using some AXI4 SOC demonstration examples.

What you will learn:

  • Introduction to NVIDIA MatchLib
  • What is motivating a change in design and verification flow
    complexity
  • How risk/complexity in many of today’s SOCs differs from the past
  • How to write HLS models using NVIDIA MatchLib
  • How Matchlib significantly improves simulation speed and
    verification efficiency
  • Where to find more information and examples for MatchLib from
    Siemens EDA and NVIDIA

Who should view:

  • RTL designers, hardware architects, and managers interested in
    moving up to HLS

Seznamte se s přednášejícím

Siemens EDA

Stuart Swan

HLS Technologist

Stuart Swan is an HLS Technologist in the Catapult team, focusing on SoC modeling for High-Level Synthesis. Prior to Siemens EDA, Stuart worked for Qualcomm and Cadence. Stuart is co-author of the first book on SystemC, "System Design with SystemC," and was the IEEE technical chairman of the 2005 SystemC LRM. He received his BSEE from Stanford University.