webinář na vyžádání

Cornell University: Building Sparse Linear Algebra Accelerators with HLS

Odhadovaná doba sledování: 72 min

Sdílení

Cornell intros HiSparse: accelerator on sparse-matrix dense-vector multiplication. Using both HLS implementation and simulation, their sparse accelerators deliver promising speedup with increased bandwidth and energy efficiency.

Sparse linear algebra (SLA) operations are essential in many applications such as data analytics, graph processing, machine learning, and scientific computing. However, it is challenging to build efficient hardware accelerators for SLA operations since they typically exhibit low operational intensity and irregular compute and data access patterns. In particular, some of these challenges are not well studied in the context of High-Level Synthesis (HLS). 
 
In this talk, we first introduce HiSparse, an accelerator on sparse-matrix dense-vector multiplication (SpMV). To achieve a high bandwidth utilization, we co-design the sparse storage format and the accelerator architecture. We further demonstrate the use of Catapult HLS to build a high-throughput pipeline that can handle irregular data dependencies and access patterns. Building on our SpMV accelerator, we further develop a versatile sparse accelerator that can support multiple SLA operations with run-time configurability to support different compute patterns. Our architecture design is guided by a novel analytical model which enables rapid exploration of the design configuration search space. According to our evaluation using both HLS implementation and simulation, our sparse accelerators deliver promising speedup with increased bandwidth and energy efficiency when compared to CPU and GPU executions.

Seznamte se s přednášejícím

Cornell University

Yixiao Du

Ph.D. student

Yixiao is a second-year Ph.D. student at Cornell Computer Systems Lab, advised by Prof. Zhiru Zhang. His current research interests include efficient acceleration of sparse workloads with high-level synthesis. He received his bachelor’s degree in Microelectronics Science and Engineering from the University of Electronic Science and Technology of China.

Související zdroje informací

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.