Offshore Asgard Subsea Compression was successfully brought on stream in September 2015 boosting the gas pressure from the Midgard and Mikkel fields. Going forwards with project phase 2, a possibility to increase the pressure ratio has been identified by means of introducing wet gas compression which is achieved by purposely injecting liquid upstream of each compressor.
This presentation will cover a co-operation between Aker Solutions and Equinor initiated with the goal of determining how a multiphase flow split can be predictively modelled with Simcenter™ STAR-CCM+™ software in the subsea framework. Measurements from subsea operations will be compared to purpose built Computational Fluid Dynamics (CFD) models showing how high-fidelity simulations in Simcenter STAR CCM+ today can be used to predict the complex mechanisms behind a three-phase uneven flow split.
Speaker: Andreas Martinsson

CFD 工程专家
安德烈亚斯·马丁森主要负责 Aker Solutions 的 CFD 领域多相流和热应用。自 2012 年加入 Aker Solutions 以来,他一直致力于 CFD 的应用研究,希望将其发展成为一个极具价值的工具,应用于从井口到水上处理系统的整个产品组合。