点播式网络研讨会

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

预估观看时长:31 分钟

分享

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc. HLS tools are expected to synthesize this code to RTL which can be input to the traditional RTL downstream flow (RTL / GDS) RTL lint / formal check tools cannot be run on HLS RTL (as the errors cannot be correlated to HLS source code) Onespin systemC/C++ extension DV help to overcome this challenge. This session will be presented by Siemens on behalf of Infineon Technologies AG.

主讲嘉宾简介

Siemens EDA

Vlada Kalinic

SystemC Product Specialist

Vlada Kalinic is the SystemC Product Specialist at Siemens EDA, and is involved in the evaluations with the new customers as well supporting the current portfolio of the customers to improve the current SystemC flows. Vlada has also another role, as Product Specialist of EC-FPGA in OneSpin. Vlada holds a master’s degree with honors in Electrical and Computer Engineering, Embedded Systems and Algorithms from the University of Novi Sad (Serbia). Prior to Mentor/Siemens, Vlada worked with OneSpin for 5+ years and was involved in various successful evaluations with SystemC and EC-FPGA customers.

相关资源

面向工业机械的高级规划和调度 (APS)
E-book

面向工业机械的高级规划和调度 (APS)

通过高级规划和调度软件获得更好的可见性并改进制造工艺。阅读电子书,了解更多信息。

为数字化时代实现电子业务转型
Webinar

为数字化时代实现电子业务转型

观看我们的点播式网络研讨会,了解电子制造商如何实施成功的数字化转型战略,从而增强协作、提高效率并推动创新。