点播式网络研讨会

通过集成式端到端结构开发流程加快适航认证

预估观看时长:46 分钟

分享

通过集成式端到端结构开发流程加快适航认证

Aircraft manufacturers can suffer major delays on their programs due to non-recurring costs spent on structural development. Knowing that up to 60% of aircraft non-recurring costs can be spent on the structural development and achieving airworthiness certification, any improvement will have a significant impact.

This webinar discusses how Bye Aerospace (BA) is developing their all-electric eFlyer 2 using an integrated end-to-end structural development process, which helps achieve faster certification. More specifically, BA will show how a model-based primary structure use case is coupled with BA-developed innovative design techniques that enable shorter multidisciplinary design cycles. This speedup is possible through seamless exchange of design and analysis data.

Additionally, we will show how such an integrated end-to-end process can be extended to:

  • Margin of safety calculations with traceable certification reports
  • Flutter simulation tied to the CAD model
  • Material characterization, particularly for composite structures to virtually characterize the material behaviors and significantly reduce composite material development time

主讲嘉宾简介

Bye Aerospace

Daniel Hinson

首席复合材料结构工程师

相关资源

多领域集成中的数字线程
Webinar

多领域集成中的数字线程

了解数字线程如何在多领域得以保持并提供集成式自动化电气设计环境。

整体工程:如何开发强大的 E/E 系统
Webinar

整体工程:如何开发强大的 E/E 系统

使用西门子整体产品开发工具创建强大的 E/E 系统。

将 Capital E/E 系统开发解决方案集成到电动汽车开发中
Infographic

将 Capital E/E 系统开发解决方案集成到电动汽车开发中

实施 Capital E/E 系统开发解决方案,以设计电动汽车开发中的集成、安全和验证。了解更多信息