点播式网络研讨会

通过集成式端到端结构开发流程加快适航认证

预估观看时长:46 分钟

分享

通过集成式端到端结构开发流程加快适航认证

Aircraft manufacturers can suffer major delays on their programs due to non-recurring costs spent on structural development. Knowing that up to 60% of aircraft non-recurring costs can be spent on the structural development and achieving airworthiness certification, any improvement will have a significant impact.

This webinar discusses how Bye Aerospace (BA) is developing their all-electric eFlyer 2 using an integrated end-to-end structural development process, which helps achieve faster certification. More specifically, BA will show how a model-based primary structure use case is coupled with BA-developed innovative design techniques that enable shorter multidisciplinary design cycles. This speedup is possible through seamless exchange of design and analysis data.

Additionally, we will show how such an integrated end-to-end process can be extended to:

  • Margin of safety calculations with traceable certification reports
  • Flutter simulation tied to the CAD model
  • Material characterization, particularly for composite structures to virtually characterize the material behaviors and significantly reduce composite material development time

主讲嘉宾简介

Bye Aerospace

Daniel Hinson

首席复合材料结构工程师

相关资源

通过实时可见性和控制性提高质量
E-book

通过实时可见性和控制性提高质量

通过低代码提高电子和半导体制造的质量和效率。获得实时可见性、共享 KPI 并优化生产,从而更快、更明智地做出决策。

低代码解决方案如何加速工业机械制造
E-book

低代码解决方案如何加速工业机械制造

了解 Mendix 等低代码解决方案如何帮助工业机械制造商加速数字化转型、应对复杂性并优化设计、制造和服务运营。