点播式网络研讨会

Spacecraft acoustic testing

Reverberation or direct field acoustic noise testing of space hardware

预估观看时长:64 分钟

分享

Example of spacecraft acoustic testing using direct field acoustic noise testing

The objective of spacecraft acoustic testing is to demonstrate the ability of the structure and avionics to withstand the broadband random acoustic environment experienced within the launch vehicle payload fairing. This webinar looks at secure space hardware testing using reverberation or direct field acoustic noise testing (DFAN).

Learn about closed-loop control solutions for operation in reverberation rooms and direct-field environments to implement robust, state-of-the-art control algorithms that provide spatial uniformity of sound pressure levels within tight tolerances.

Several layers of security controls help prevent any over-testing of the very valuable payload. Moreover, an innovative pre-test analysis assists the user in defining the optimal control parameters to ensure a safe, time- and energy-efficient workflow.

Why is spacecraft acoustic testing necessary?

Spacecraft acoustic testing is necessary to prove that your design is strong enough to withstand the launch. It is a mission-critical task to validate the design against vibration, shock and acoustic loads. It has to be designed right the first time because there is no second chance if elements of a spacecraft are damaged or destroyed as a result of the hostile environment that is created during the launch.

Acoustic qualification testing of space hardware includes two methods. Reverberant field acoustic noise testing is the traditional test, existing for decades, performed in a reverberant chamber. The objective is to test-validate hardware to guarantee launch survivability by accurately reproducing acoustic loads in a reverberation room controlling excitation spectra of multiple acoustic modulators using feedback from microphones around the structure while monitoring hundreds of vibration and strain responses.

Direct field acoustic noise (DFAN) testing is an alternative, innovative technique for spacecraft acoustic testing. DFAN uses loudspeakers to create the acoustic field using a narrow-band, multiple-input multiple-output (MIMO) control technique. Watch the webinar to learn more.

Methods for spacecraft acoustic testing

You will learn:

  • How to perform acoustic qualification of space structures
  • Benefits of reverberant and DFAN approaches
  • How to ensure maximum spacecraft protection during qualification tests

主讲嘉宾简介

Siemens Digital Industries Software

Mostapha Choukri

Senior Business Development Manager, Simcenter Testing Solutions

相关资源

采用加速工程设计解决方案为小型企业带来的优势
Video

采用加速工程设计解决方案为小型企业带来的优势

采用加速工程设计解决方案为小型企业带来的优势

面向中小企业 (SMB) 的加速工程解决方案
E-book

面向中小企业 (SMB) 的加速工程解决方案

西门子加速工程 (AE) 解决方案可助力中小型企业加快产品上市速度并提高产品质量。阅读此电子书,了解更多相关信息。

从概念到制造的设计师之旅
Infographic

从概念到制造的设计师之旅

了解设计师使用西门子数字化工业软件从概念到制造之旅的 4 个完整步骤。