вебінар на вимогу

Hailo achieves unprecedented AI performance using Aprisa digital implementation flow

Поширити

Blue futuristic circuit board for AI performance with binary numbers

Elyasaf Munk, Physical Design Engineer at Hailo Technologies, presents "High Quality Designs with Fast Design Closure". Elyasaf shares his experience using Aprisa to achieve low cost and low power on the world’s top performing AI processor for edge devices. With Aprisa, Hailo was able to achieve 90% cell utilization, drastically reducing the size of their chip and lowering their cost. Hailo’s strict dynamic power requirements were also handled well by Aprisa without sacrificing on performance.

About Hailo

Hailo’s mission is to enable smart edge technologies reach their full potential. The solution Hailo presents bridges the gap between existing and future AI technologies and the compute capacity needed to power these applications. The company is focused on building AI processors efficient and compact enough to compute and interpret vast amounts of data in real-time—processors that can be embedded in the edge devices themselves. Now, complicated AI applications that could previously only run on the cloud are made possible to run on the edge, and the best part– with a fraction of the power consumption. See how Aprisa helps Hailo achieve their ultra low-power, compact AI processors for edge devices.

Пов'язані ресурси