вебінар на вимогу

Achieve EMC compliance for electrified vehicles with electromagnetic simulation

Support electric vehicle design and verification using EMC simulation

Приблизний час перегляду: 41 хвилин

Поширити

Full 3D model of the vehicle and electric wire harness used to understand EMC concerns for EV safety and reliability

The number of electrical components in the automotive industry has grown exponentially over the past 60 years. But with the fierce development of the electric vehicle, electrified propulsion has led to high-voltage emissions and an increased number of wireless signal and data transmissions. Automakers must address the critical challenge of electromagnetic compatibility (EMC) to ensure electric vehicles are safe and reliable.

Discover how OEM engineering departments can support electric wire harness design and verification using simulation in this on-demand webinar.

Solve EMC challenges with Simcenter simulation software

New power electronics system designs based on materials such as gallium nitride (GaN) are emerging, aiming at a higher level of performance. However, these new technologies also come with new EMC challenges and must be accurately understood. The Siemens Xcelerator portfolio is unique regarding electrified vehicle EMC analysis as it provides design and verification capabilities of all key electrical powertrain system components at different levels of abstraction. It also provides the tools needed for circuital electrical simulation of electric powertrain systems so that engineers can simulate the critical electrical currents up to several 100MHz in critical cables.

Utilize a comprehensive digital twin to address EM noise radiation

Electrification will introduce unwanted electromagnetic (EM) noise and affect EMC. When a system is compliant with EMC requirements, it functions correctly within its electromagnetic environment: the system is sufficiently immune to EM influences, both from outside and originating within itself. Using Siemens Simcenter solutions, engineers can build a full vehicle-level 3D model or digital twin, including wire harnesses with the highest EMC accuracy. With this integrated set of capabilities, engineers can adequately understand and mitigate EMC concerns efficiently and effectively.

Discover simulation tools that help engineers understand the propagation of EM energy from the source to the victims to mitigate problems earlier in development — Watch the webinar now!

Зустрітися зі спікерами

Siemens Digital Industries Software

Koen de Langhe

Director of Product Management, Simcenter Electronics Systems Simulation

Koen De Langhe carries 25 years of expertise in the area of CAE, primarily 3D mechanical analysis: Structural Dynamics, Acoustics, NVH analysis and since several years as well solutions for Electromagnetics including Motors, Transformers, EMC/EMI, antenna and radar.

Within Product Management, Koen is setting the product strategy and roadmap for a range of 3D simulation products and bringing existing products to the market and to customers.

Siemens Digital Industries Software

Erica Van Berkum

Senior Product Manager, Capital Electrical Distribution

Erica has more than 20 years of diverse automotive-industry experience, ranging from wire harness design and electrical component implementation, to software deployment. Erica is responsible for the strategy and roadmap of the Capital Electrical design tools for E/E system development.

Пов'язані ресурси