spletni seminar na zahtevo

Veloce X-STEP optimizes O-RAN interoperability and conformance

Delite

Veloce X-STEP optimizes O-RAN interoperability and conformance

In this webinar, we introduce the *Veloce™ X-STEP™ platform*, which is a fiber optic test system radio base station system designed with the highest possible timing accuracy and protocol configurability in mind. The patented Veloce X-STEP architecture allows full configurability of transmitted data full visibility into received data, even in the case of erroneous packets.

Along with the introduction of eCPRI and O-RAN in its wide protocol portfolio, Veloce X-STEP can be used in the testing and development of 5G Fronthaul devices and networks. Veloce X-STEP can operate as a monitor to O-RAN C/U/S/M-plane traffic in quality and interoperability assurance, or as an emulator of the O-DU or O-RU, generating O-RAN traffic for the other part. Multilink support in Veloce X-STEP significantly increases testing efficiency and allows synchronized captures from separate fibers.

The session will highlight several practical use cases from O-RAN management, sync, control, and user planes that need special attention in the verification phase to ensure seamless integration of the fronthaul network.

Veloce X-STEP optimizes O-RAN interoperability and conformance,

highlights several practical use cases from O-RAN management, sync,
control, and user planes that need special attention in the
verification phase to ensure seamless integration of the fronthaul
network.