The authors present the adoption of SystemC for High-Level-Synthesis replacing the traditional RTL design flow. A steady increase in the need for connectivity in the automotive industry and the resulting higher complexity in the individual ASICs requires a novel methodology within the ASIC design phase. This is now being implemented using a new design flow starting from an abstract network simulation in SystemC down to either FPGA-Prototyping (simulating a complex network topology) or the tapeout RTL for an individual ASIC. In conclusion, the authors will present the ease of use and the value-add of the HLS methodology in an automotive context.

Meet the Speakers

INOVA Semiconductors

Fabian Kluge

Systems Engineering Manager

Fabian Kluge is a Systems Engineering Manager at INOVA Semiconductors, working on architectures and concepts for new automotive serializers and networking products, now adopting SystemC as a modelling language. He has a strong background in FPGA and general electronics development including various high-speed interfaces. He received his master’s degree in electrical engineering from Technical University Munich in 2017, specializing in EDA and radar technologies.

Coseda

Thomas Arnt

Application Engineering Manager

Thomas Arndt is an Application Manager at COSEDA Technologies, focusing on system level design and simulation solutions. He has over 20 years of experience in the chip design and the EDA industry. His particular areas of expertise are in the field of digital as well as analog system design, simulation and High-Level Synthesis. Prior to joining COSEDA, he was working at the Fraunhofer Institute for Integrated Circuits, one of the largest research institutions in the field of design automation in Europe. He received his diploma in electrical engineering from the Technical University of Dresden.

Conteúdo informativo relacionado

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.