webinar na żądanie

Early AXI4 SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS

Szacowany czas: 24 min

Udostępnij

Early AXI SOC Performance Verification Using NVIDIA MatchLib and Catapult HLS

NVIDIA Matchlib is a new open source library that enables much faster design and verification of SOCs using High-Level Synthesis (HLS). One of the primary objectives of Matchlib is to enable performance accurate modeling of SOCs in SystemC/C++. With these models, designers can identify and resolve issues such as bus and memory contention, arbitration strategies, and optimal AXI4 interconnect structure at a much higher level of abstraction than RTL. In addition, much of the system level verification of the SOC can occur in SystemC/C++, before RTL is even created. Once the architectural performance is verified, this flow provides a fully automated flow to silicon using Catapult HLS. This webinar will introduce NVIDIA Matchlib and its usage with Catapult HLS using some AXI4 SOC demonstration examples.

What you will learn:

  • Introduction to NVIDIA MatchLib
  • What is motivating a change in design and verification flow
    complexity
  • How risk/complexity in many of today’s SOCs differs from the past
  • How to write HLS models using NVIDIA MatchLib
  • How Matchlib significantly improves simulation speed and
    verification efficiency
  • Where to find more information and examples for MatchLib from
    Siemens EDA and NVIDIA

Who should view:

  • RTL designers, hardware architects, and managers interested in
    moving up to HLS

Poznaj naszego eksperta

Siemens EDA

Stuart Swan

HLS Technologist

Stuart Swan is an HLS Technologist in the Catapult team, focusing on SoC modeling for High-Level Synthesis. Prior to Siemens EDA, Stuart worked for Qualcomm and Cadence. Stuart is co-author of the first book on SystemC, "System Design with SystemC," and was the IEEE technical chairman of the 2005 SystemC LRM. He received his BSEE from Stanford University.

Powiązane treści

Ogranicz ryzyko wystąpienia błędów projektowych o 25%
Case Study

Ogranicz ryzyko wystąpienia błędów projektowych o 25%

Carraro Group korzysta z oprogramowania VeSys, aby o połowę skrócić testy funkcjonalne...