실시간 웨비나

Glass-Weave Skew Part II: mitigation methods

Understanding and controlling sources of differential-pair skew is critical to signal integrity and reduces the potential for nightmarish field failures.

2022년 11월 30일 오전 11:00 협정 세계시
2022년 11월 30일 오후 09:00 협정 세계시

공유

differential pair skew caused by Glass-Weave Skew

Differing micro-environments can cause slight signal delays within a differential pair, leading to apparently random field failures in production. This is known as Glass-Weave Skew, a phenomena that's easier to prevent that predict.

A serial link’s differential-skew budget shrinks as bit rates increase. For example, a 1 Gbps (500 MHz) signal would have roughly 250 ps of skew tolerance. That’s a wide window, and why most engineers didn’t need to worry about GWS 20+ years ago.

In this webinar we explore eleven possible solutions to help prevent glass-weave skew, with an eye toward manufacturing costs and future-proofing your designs.

The webinar covers

  • Deterministic methods for addressing GWS
  • Probabilistic GWS mitigation methods
  • Glass styles and their relative suitability for mitigating GWS

발표자 소개

Z-zero

Bill Hargin

CEO

Bill Hargin is the chief everything officer at Z-zero, developer of the PCB stackup design and material selection software, Z-planner Enterprise. Bill is an industry pioneer, with more than 25 years working in PCB signal integrity and manufacturing, while authoring dozens of articles on signal integrity, stackup design, and material selection. Hargin is also the author of the iConnect007 publication Stackups, the Design within the Design, a regular columnist for Printed Circuit Design and Fabrication magazine, and a contributing author for the Printed Circuits Handbook.

Bill is a regular speaker and panelist at both DesignCon and PCB West, and more than 10,000 engineers and PCB designers worldwide have taken his workshop on high-speed PCB design. Mr. Hargin served as director of marketing for Mentor Graphics’ HyperLynx SI software and as the Director of North American Marketing for Nan Ya Plastic’s PCB laminate division in Taiwan before founding Z-zero.

관련 자료

중장비 내부 편의성 및 안전
White Paper

중장비 내부 편의성 및 안전

Siemens 스마트 솔루션은 중장비의 내부를 개선하여 작업자의 편의성과 안전성을 높이는 동시에 개발 시간을 줄이도록 지원합니다.

시뮬레이션을 활용하여 ICE에서 전기 모터로 변환하는 시저 리프트 성능 개선 지원
Case Study

시뮬레이션을 활용하여 ICE에서 전기 모터로 변환하는 시저 리프트 성능 개선 지원

Haulotte는 Simcenter를 사용하여 Pulseo 리프트의 최대 작업 높이를 25%, 적재 용량을 50% 향상합니다

예측 모델링 소프트웨어로 고성능 설계 구현
Video

예측 모델링 소프트웨어로 고성능 설계 구현

예측 모델링 소프트웨어를 사용하여 메카트로닉 복잡성을 관리하고 엔지니어링 프로세스를 개선합니다. 자세히 알아보십시오.