온디맨드 웨비나

Copper Roughness and Signal Integrity

What you need to know

예상 소요 시간: 45분

공유

Cu rougness and SI for your PCB

There's been a lot of talk over the years regarding copper roughness, yet few hardware engineers or signal integrity practitioners have a detailed understanding of this key contributor to high-speed signal loss.

To keep you from getting surprised by previously untracked contributors to insertion loss, we will discuss 10 critical things you need to know about copper roughness and their impact on board costs and signal integrity.

  1. There’s no standard terminology governing copper roughness — it’s left to individual vendors
  2. High speed materials use primary/secondary/tertiary copper foil types — at different price points
  3. There are multiple ways to measure roughness
  4. There are several ways to model loss mathematically — which one is best?
  5. Loss from copper roughness is more controllable than skin effect
  6. Understanding prepreg/process - side roughness
  7. There are multiple fabricator process treatments that affect roughness
  8. Foil selection dominates loss, as compared to process treatments
  9. Plating’s effect on copper roughness
  10. Practical advice for managing roughness, loss, and cost

발표자 소개

Z-zero

Bill Hargin

CEO

Bill Hargin is the chief everything officer at Z-zero, developer of the PCB stackup design and material selection software, Z-planner Enterprise. Bill is an industry pioneer, with more than 25 years working in PCB signal integrity and manufacturing, while authoring dozens of articles on signal integrity, stackup design, and material selection. Hargin is also the author of the iConnect007 publication Stackups, the Design within the Design, a regular columnist for Printed Circuit Design and Fabrication magazine, and a contributing author for the Printed Circuits Handbook.

Bill is a regular speaker and panelist at both DesignCon and PCB West, and more than 10,000 engineers and PCB designers worldwide have taken his workshop on high-speed PCB design. Mr. Hargin served as director of marketing for Mentor Graphics’ HyperLynx SI software and as the Director of North American Marketing for Nan Ya Plastic’s PCB laminate division in Taiwan before founding Z-zero.

관련 자료

Smart Biosphere 애플리케이션으로 시장 출시 시간을 72% 단축
Case Study

Smart Biosphere 애플리케이션으로 시장 출시 시간을 72% 단축

Biosphere Foundation은 Insights Hub와 Mendix를 사용하여 자연을 모니터링 및 복원하고 기후 비상 사태를 해결합니다

자동차 제조업체, 도장 공장의 처리량 15% 증가
Case Study

자동차 제조업체, 도장 공장의 처리량 15% 증가

Insights Hub 및 플랜트 시뮬레이션 IoT 데이터 분석을 사용하여 생산 감소의 근본 원인을 파악하는 MGI