온디맨드 웨비나

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

예상 소요 시간: 20분

공유

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

Deep Learning algorithms are rapidly evolving, with new techniques and architectures being proposed on a regular basis. This poses a significant challenge for hardware design. These algorithms often require specialized hardware accelerators for efficient execution. However, the design cycle for these accelerators is complex and time-consuming, as it involves a significant effort to master the algorithm and implement an appropriate hardware architecture. As new DL algorithms emerge, existing hardware accelerators may become obsolete or may not be able to integrate the latest optimizations. This leads to a significant gap between newly emerging algorithms and available hardware accelerators. To address this problem, High-Level Synthesis (HLS) use has increased to accelerate the design process and bridge the gap between software and hardware design by describing the desired behavior of the accelerator in a high-level programming language (e.g. C++). We present a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms. By proposing a new automatic synchronization, we were able to balance the execution time of all convolutional layers in MobileNet-v1 to achieve a pipelined hardware architecture capable of handling 500 fps.

발표자 소개

CEA List (French Alternative Energies and Atomic Energy Commission)

Nermine Ali

PhD - Research Engineer

Nermine Ali is a research engineer at CEA List (French Alternative Energies and Atomic Energy Commission), France, in the field of embedded systems and artificial intelligence, since December 2021. She received her PhD Degree in Electronics from Université de Bretagne-Sud, France, in 2022. Her current research interests include hardware designs for neural networks applications and high-level design flows including High-Level Synthesis tools to exploit fast exploration and hardware generation.

관련 자료

비즈니스 성장에 따라 확장 가능하도록 제작된 Teamcenter X 클라우드 PLM
Video

비즈니스 성장에 따라 확장 가능하도록 제작된 Teamcenter X 클라우드 PLM

Teamcenter X가 언제 어디서나 팀이 작업할 수 있도록 제품 개발 및 제공을 지원하는 클라우드 PLM을 통해 소규모 스타트업의 성장을 어떻게 지원하는지 알아보십시오.