온디맨드 웨비나

Using simulation to develop a hydrogen fuel cell propulsion system

Exploring the use of simulation to develop a commercially viable hydrogen fuel cell propulsion system for aircraft

예상 시청 시간: 58분

공유

Man looking at laptop next to airplane part

The aviation industry is currently responsible for three percent of global CO2 emissions. To achieve the goal of climate-neutral aviation, it is essential to develop and implement new technologies that can reduce the carbon footprint of air travel. One promising solution is the use of hydrogen fuel cells as a propulsion system for aircraft. Simulation allows us to test and optimize the design of the propulsion system in a virtual environment, reducing the time and cost required to bring the technology to market. In this webinar, we will explore the use of simulation to develop a commercially viable hydrogen fuel cell propulsion system for aircraft.

Topics covered will include:

  • The main advantages of hydrogen fuel cell compared to other approaches toward climate-neutral aviation
  • The main challenges when it comes to the propulsion system
  • Fuel cell system development – the multiple stacks balance of plant (BOP) which makes the fuel cell perform
  • The use of Simcenter simulation technology to develop and optimize the design of the propulsion system in a virtual environment, reducing the time and cost required to bring the technology to market.

발표자 소개

Siemens Digital Industries Software

Jens de Boer

Simcenter Solution Manager for Aerospace

Jens는 열정적인 항공우주 엔지니어입니다. 그는 지난 14년 동안 Siemens에서 근무하면서 여러 항공우주 회사들과 협력하여 개발 주기 전반에 걸쳐 시뮬레이션 및 테스트 프로세스를 채택하고 간소화했습니다.

Siemens Digital Industries Software

Stéphane Mouvand

Aerospace Business Development Manager, Simcenter System Simulation

Stéphane은 2005년 주요 항공우주 분야 고객의 영업 담당자로 Siemens에 합류했습니다. 현재는 Simcenter 시스템 시뮬레이션 솔루션을 위한 항공우주 및 방위 사업 개발을 이끌고 있습니다.

Ricardo Ltd.

Tom Stokes

Project Engineer, Analysis and Simulation

Tom started his career with Ricardo in 2019 after graduating from Loughborough University with a master’s degree in Automotive Engineering. His studies there were primarily focused on engine performance simulation.
After university, Tom joined Ricardo in the Simulation and Analysis team, where his focus has increasingly shifted towards the use of hydrogen both as a fuel for internal combustion engines and hydrogen fuel cells.

관련 자료