オンデマンド・ウェビナー

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis

Towards Physical Prototype

視聴時間の目安: 26 分

共有

Infineon & Coseda present on the adoption of High-Level-Synthesis at an existing SystemC system level model.

Infineon & Coseda present on the adoption of High-Level-Synthesis at an existing SystemC system level model. Discussing the use-case of using HLS for fast prototyping of a purely hardware signal path model, with focus on the required adaptations since the model was initially developed without having HLS in mind. Furthermore the audience will understand the required refinement steps (e.g. quantization, handshake between modules, applying required constraints) needed to synthesize the optimized RTL. In conclusion they will present the ease of use and the value of the HLS methodology in an industrial project.

講演者の紹介

Infineon Technologies AG

Ana Maria Plaisenanu

Firmware Staff Engineer

Ana Plaiseanu is a Firmware Engineer at Infineon Technologies Romania - Sense & Control Division, working mainly on firmware development and testing for Automotive ASIC products but with an interest also in behavioral modeling and testing for automotive sensors. Ana received her bachelor degree from Polyethnic University of Bucharest, specializing in microelectronics and has a 9 year experience as Software & Firmware Engineer in automotive product lines for pressure and magnetics sensors.

Coseda

Thomas Arnt

Application Engineering Manager

Thomas Arndt is an Application Manager at COSEDA Technologies, focusing on system level design and simulation solutions. He has over 20 years of experience in the chip design and the EDA industry. His particular areas of expertise are in the field of digital as well as analog system design, simulation and High-Level Synthesis. Prior to joining COSEDA, he was working at the Fraunhofer Institute for Integrated Circuits, one of the largest research institutions in the field of design automation in Europe. He received his diploma in electrical engineering from the Technical University of Dresden.

関連情報

Simcenter 3Dの評価版
Trial

Simcenter 3Dの評価版

Simcenter 3Dは、現在市販されているなかで最も包括的な完全統合型のCAEソリューションであり、シミュレーション効率を飛躍的に向上させることによって、複合領域にわたる複雑な製品の性能エンジニアリングを実現します。

Simcenter Testlab Neo評価版
Trial

Simcenter Testlab Neo評価版

Simcenter Testlab Neoの無償評価版を使用して、テストデータの視覚化、処理、知見の取得がいかに容易かを体験できます。

オンラインでの設計シミュレーション
Trial

オンラインでの設計シミュレーション

・ NX設計環境内で直接シミュレーションを実行することにより、開発期間を短縮し、コストを削減 ・ 設計中に構造、熱、機構性能に関する製品挙動を予測 ・ 設計を迅速に反復し、設計変更が製品性能に与える影響を素早く把握 ・ NXでシミュレーションを自分で簡単に実行できることを、わかりやすい例で学ぶ

統合型設計/シミュレーション
Trial

統合型設計/シミュレーション

• 複合領域にまたがるデータを使用して正確なデジタル・ツインを作成し、開発のあらゆる段階で機械の性能を予測します。 •3D CADおよびCAEが組み込まれた単一環境を活用し、高解像度モデルを生成した後、異なるオペレーション・ポイントで機械の安定性をすばやく調査します。 •強力なシステム・シミュレーション・プラットフォームを使用して、複雑なシステムのコンポーネントのサイズを正確に設定します。 •最先端の音響シミュレーション技術を使用して、顧客の要件と安全規制…