オンデマンド・ウェビナー

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

視聴時間の目安: 20 分

共有

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

Deep Learning algorithms are rapidly evolving, with new techniques and architectures being proposed on a regular basis. This poses a significant challenge for hardware design. These algorithms often require specialized hardware accelerators for efficient execution. However, the design cycle for these accelerators is complex and time-consuming, as it involves a significant effort to master the algorithm and implement an appropriate hardware architecture. As new DL algorithms emerge, existing hardware accelerators may become obsolete or may not be able to integrate the latest optimizations. This leads to a significant gap between newly emerging algorithms and available hardware accelerators. To address this problem, High-Level Synthesis (HLS) use has increased to accelerate the design process and bridge the gap between software and hardware design by describing the desired behavior of the accelerator in a high-level programming language (e.g. C++). We present a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms. By proposing a new automatic synchronization, we were able to balance the execution time of all convolutional layers in MobileNet-v1 to achieve a pipelined hardware architecture capable of handling 500 fps.

講演者の紹介

CEA List (French Alternative Energies and Atomic Energy Commission)

Nermine Ali

PhD - Research Engineer

Nermine Ali is a research engineer at CEA List (French Alternative Energies and Atomic Energy Commission), France, in the field of embedded systems and artificial intelligence, since December 2021. She received her PhD Degree in Electronics from Université de Bretagne-Sud, France, in 2022. Her current research interests include hardware designs for neural networks applications and high-level design flows including High-Level Synthesis tools to exploit fast exploration and hardware generation.

関連情報

未来をエンジニアリング:  生産/工作機械産業を動かすトレンド
E-book

未来をエンジニアリング: 生産/工作機械産業を動かすトレンド

産業エンジニアリングの未来を方向づける最新のトレンドを探り、仮想の設計検証テストがいかに重要な役割を担っているのかご確認ください。

機械メーカーに加速的な変化をもたらす技術イノベーション
White Paper

機械メーカーに加速的な変化をもたらす技術イノベーション

スマートなコネクテッドマシンとシーメンスの包括的なデジタル・ツインで競争優位性を獲得