Webinar on-demand

Combining system simulation and 3D CFD for cardiac haemodynamic modeling

Best practices for CFD haemodynamic modeling with Simcenter STAR-CCM+

Tempo di visione stimato: 49 minuti

Condividi

Slide titled “Best practices for CFD haemodynamic modeling of an AVF” with a graph measuring velocity magnitude

Simulation is long established as a method for generating proof that a medical device meets a requirement. But simulation can be used in other ways as well. Watch the on-demand webinar to learn about best practices for computational fluid dynamics (CFD) haemodynamic modeling and how other organizations have used simulation for diagnosis and intervention planning.

Build a credible model for CFD haemodynamics

Simulation is not useful unless it is credible. There must be trust in the predictive capabilities of a computational model in the specific context of where it is being used. Once that credibility is established, organizations can use simulation all throughout the design lifecycle. From early concept building where costs are relatively low, simulation can help to reduce the number of prototypes needed and therefore the ability to get a product to market sooner.

Achieve detailed analysis of the haemodynamic environment and metrics

The majority of CFD haemodynamic studies use velocity inlet–pressure outlet boundary conditions. The inlets are prescribed to be the velocity or mass flow waveforms. In regard to outlets, there are a few options, including zero-pressure or “bleeding out” outlet, prescribed flow split percentages based on daughter vessel areas, or Windkessel models. Lastly, for walls, non-slip conditions versus fluid-structure interaction methods can be used.

What you will learn from this webinar

  • How to implement best practices for CFD haemodynamic modelling in Simcenter STAR-CCM+
  • How to compute key haemodynamic metrics within Simcenter STAR-CCM+
  • How to automate a repeatable and efficient CFD pre-processing pipeline
  • How to couple Simcenter Amesim and Simcenter STAR-CCM+ for zero-dimensional Windkessel models

Relatori

Siemens Digital Industries Software

Javier Garriz

Solution Consultant for Medical Devices

University of Strathclyde, Glasgow, UK

George Hyde-Linaker

Department of Biomedical Engineering

University of Strathclyde, Glasgow, UK

Dr. Asimina Kazakidi, FHEA, MIPEM, RSE ΜYAS

Senior Lecturer, Director of MSc/MRes programmes in Biofluid Mechanics

Risorse correlate

Migliorare la gestione della qualità nel settore automotive
Infographic

Migliorare la gestione della qualità nel settore automotive

Collega i processi di gestione della qualità tipicamente scollegati e supera le sfide del settore applicando tecnologie innovative con le soluzioni Smart Manufacturing di Siemens. Maggiori informazioni

Best practice dei sistemi PLM e QMS
White Paper

Best practice dei sistemi PLM e QMS

Le soluzioni Siemens per la gestione della qualità (QMS) aiutano i clienti a colmare il divario tra ruoli e attività al fine di migliorare la collaborazione.

Ottimizzare la gestione della qualità e della conformità con l’utilizzo di best practice
White Paper

Ottimizzare la gestione della qualità e della conformità con l’utilizzo di best practice

Le soluzioni Siemens per la gestione della qualità (QMS) aiutano i clienti a colmare il divario tra ruoli e attività al fine di migliorare la collaborazione.