webinar na zahtjev

Renesas Electronics: Ultra-low-power number recognition: Rapid prototyping with Catapult AI NN

Procijenjeno vrijeme gledanja: 15 minute

Podijeli

Renesas logo

Bringing AI models to custom silicon traditionally requires long design cycles and complex hardware design flows. As AI moves toward energy-constrained edge systems, there is increasing demand for approaches that enable both rapid prototyping and strong hardware quality-of-results.

This talk presents the development of a neural network inference accelerator created during the Accelerating Inferencing Using HLS Hackathon organized by Siemens EDA. Starting from a Python model trained on the MNIST dataset, the system was optimized across the full stack, from model tuning and post-training fixed-point quantization to architectural design and High-Level Synthesis targeting a 40 nm ASIC process. The resulting architecture integrates a dedicated inference engine with a lightweight controller based on MicroBlaze to manage data movement and execution.

Despite the rapid development cycle, the final design achieves approximately 96% classification accuracy while consuming 36 µJ per inference under strict performance and area constraints. This work demonstrates how HLS enables efficient co-optimization across the machine-learning and hardware stack, significantly shortening the path from AI models to energy-efficient silicon.

Upoznajte govornika

Renesas

Aris-Ilias Goutis

Software Engineer

Aris-Ilias Goutis is a Software Engineer at Renesas Electronics, developing C++ software tools for simulation applications. He holds a Master’s degree in Electrical and Computer Engineering from the University of Patras.

Previously, he worked as a software engineer at the Hellenic National Defense General Staff, gaining experience in complex software systems. His academic work focused on hardware architectures and AI systems, including FPGA implementations and CNN inference acceleration using High-Level Synthesis. He won 1st place in the AI ASIC Accelerator Design Hackathon by Siemens EDA, designing an AI accelerator using HLS techniques.