webinaire à la demande

Elongate shelf life of pharmaceutical ingredients using CFD indoor environment modeling

Durée estimée : 41 minutes

Partager

Employee inside cold storage of a pharmaceutical warehouse
Employee inside cold storage of a pharmaceutical warehouse

Proper storage conditions of pharmaceutics are of key importance to wholesalers in the supply chain of medicinal products between producer and retail. Computational fluid dynamics (CFD) uncovers an untapped potential within indoor temperature mapping validation of pharmaceutical warehouse facilities, as these are subject to strict governmental requirements, usually fulfilled by means of time-consuming and expensive on-site measurements.

Join us for this webinar to learn more about CFD environment modeling for pharmaceutical storage.

Pharmaceutical warehouse requirements

During construction of such a pharmaceutical warehouse facility in Denmark, Aerotak assisted in the process by mapping temperatures throughout the warehouse using Simcenter CFD solutions.

A CFD model was set up in Simcenter STAR-CCM+ and validated against temperature measurements carried out in the warehouse facility in empty conditions. The CFD model was able to capture air flow and temperature distribution in the highly stratified indoor environment to within 8% of measured values. The validated model was used to predict the temperature distribution throughout the warehouse in filled conditions, identifying local cold and hot spots that would be critical to the shelf life of the pharmaceuticals.

The value of CFD indoor environment modelling

Comparing predictions for empty and filled warehouse conditions, reduced air circulation is apparent for the filled warehouse, leading to lower temperatures near the floor of the warehouse. Based on the numerical findings and reporting for the filled warehouse condition, the proposed ventilation system was found to comply with the legislative criteria and was subsequently approved by the authorities at significant time and cost reductions for the client compared to a conventional experimental approach.

The role of computational fluid dynamics in indoor environmental modelling

Register now to attend and learn more about:

  • The value of CFD-powered temperature mapping
  • How to adopt the best practices of computational fluid dynamics in indoor environmental modeling
  • Use case examples from various industries

À propos des intervenants

Aerotak

Thomas Filholm

Managing Partner & Senior Fluid Mechanics Specialist

Aerotak

Frederik Zafiryadis

Fluid mechanics specialist

Siemens Digital Industries Software

Christofer Wanner

Portfolio Development Executive

Ressources associées

La puissance de la simulation dans la conception d'un processus de fabrication pharmaceutique
White Paper

La puissance de la simulation dans la conception d'un processus de fabrication pharmaceutique

Les solutions de gestion du cycle de vie des produits (PLM) proposées par Siemens Digital Industries Software incluent des fonctionnalités de développement de produits numérique, de fabrication numérique et de gestion des...

Discover better designs faster: Multidisciplinary simulation and design exploration in the chemical and process industry
White Paper

Discover better designs faster: Multidisciplinary simulation and design exploration in the chemical and process industry

Read this Special Report to see how companies in the Chemical and Process industry are deploying CFD simulation to predict process performance ...