tellitav veebiseminar

Coseda: High-Level Synthesis in Mixed-Signal System Context

Eeldatav Vaatamisaeg: 43 minutit

Jaga

Coseda's logo

Mixed-signal systems present unique challenges due to the coexistence of analog and digital components within a unified design. To address these challenges, high-level design methodologies are increasingly employed to manage complexity and enable early system validation. High-Level Synthesis (HLS) plays a critical role in this context by allowing designers to specify digital functionality at a higher abstraction level—such as SystemC—and automatically generate synthesizable RTL.

This presentation explores a methodology that integrates SystemC for digital modeling and SystemC AMS for analog/mixed-signal behavior, enabling holistic system-level design and simulation. By modeling the complete system at a high level, designers can validate interactions across domains, refine architectural decisions, and identify issues early in the design flow. Once verified, digital components can be synthesized using HLS, streamlining the path from algorithm to hardware. This approach promotes better abstraction, design reuse, and coherence between system-level modeling and implementation in heterogeneous mixed-signal systems.

Tutvuge kõnelejaga

Coseda

Thomas Arnt

Application Engineering Manager

Thomas Arndt is an Application Manager at COSEDA Technologies, focusing on system level design and simulation solutions. He has over 20 years of experience in the chip design and the EDA industry. His particular areas of expertise are in the field of digital as well as analog system design, simulation and High-Level Synthesis. Prior to joining COSEDA, he was working at the Fraunhofer Institute for Integrated Circuits, one of the largest research institutions in the field of design automation in Europe. He received his diploma in electrical engineering from the Technical University of Dresden.

Seotud ressursid