webinar a la carta

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

Tiempo estimado de visualización: 31 minutos

Compartir

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc. HLS tools are expected to synthesize this code to RTL which can be input to the traditional RTL downstream flow (RTL / GDS) RTL lint / formal check tools cannot be run on HLS RTL (as the errors cannot be correlated to HLS source code) Onespin systemC/C++ extension DV help to overcome this challenge. This session will be presented by Siemens on behalf of Infineon Technologies AG.

Conoce al invitado

Siemens EDA

Vlada Kalinic

SystemC Product Specialist

Vlada Kalinic is the SystemC Product Specialist at Siemens EDA, and is involved in the evaluations with the new customers as well supporting the current portfolio of the customers to improve the current SystemC flows. Vlada has also another role, as Product Specialist of EC-FPGA in OneSpin. Vlada holds a master’s degree with honors in Electrical and Computer Engineering, Embedded Systems and Algorithms from the University of Novi Sad (Serbia). Prior to Mentor/Siemens, Vlada worked with OneSpin for 5+ years and was involved in various successful evaluations with SystemC and EC-FPGA customers.

Recursos relacionados

Revoluciona tu empresa de bienes de consumo envasados con soluciones SaaS basadas en la nube
Infographic

Revoluciona tu empresa de bienes de consumo envasados con soluciones SaaS basadas en la nube

Explora los retos y las soluciones que las empresas de fabricación de bienes de consumo envasados han superado gracias al software basado en datos en la nube.

Revolución de la industria de bienes de consumo envasados: la innovadora solución de Siemens y Accenture
White Paper

Revolución de la industria de bienes de consumo envasados: la innovadora solución de Siemens y Accenture

Descubre cómo la innovadora solución de Siemens y Accenture basada en la nube revoluciona el desarrollo de productos CPG.